i.mx8M Plus Falcon mode: spl jump to kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx8M Plus Falcon mode: spl jump to kernel

ソリューションへジャンプ
3,236件の閲覧回数
mengfei
Contributor III

Dear:

I’m implementing Falcon Mode using NXP’s app note AN13709. now i successful achieve spl jump to kernel but have below error messenge. can you read it and tell me how to deal? 

the desg print the below messenge then stop

snvs_pwrkey: probe of 30370000.snvs:snvs-powerkey failed with error -22
i2c /dev entries driver

Can someone tell me where the error occurred?

my best wishes for you

mf

 

The complete printing information is as follows:

U-Boot SPL 2020.04 (Apr 20 2023 - 11:47:41 +0800)
spl_init
pmic_alloc: new pmic struct: 0x184000
pmic_get: pmic PCA9450 -> 0x184000
Bus: 0 PMIC:PCA9450 probed!
i2c_write_data: chip=0x25, len=0x0
write_data: 
i2c_write_data: chip=0x25, len=0x1
write_data:  0x29
i2c_write_data: chip=0x25, len=0x1
write_data:  0x1c
i2c_write_data: chip=0x25, len=0x1
write_data:  0x14
i2c_write_data: chip=0x25, len=0x1
write_data:  0x59
i2c_write_data: chip=0x25, len=0x1
write_data:  0x1c
i2c_write_data: chip=0x25, len=0x1
write_data:  0xa1
DDRINFO: start DRAM init
DDRINFO: cfg clk
DDRINFO: DRAM rate 4000MTS
DDRINFO: ddrc config start
DDRINFO: ddrc config done
DDRINFO:ddrphy config start
DRAM PHY training for 4000MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x0000000d]
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000002]
[PMU Major message = 0x00000001]
[PMU Major message = 0x0000000a]
[PMU Major message = 0x000000fd]
[PMU Major message = 0x000000fe]
[PMU Major message = 0x00000004]
[PMU Major message = 0x00000003]
[PMU Major message = 0x00000009]
[PMU Major message = 0x00000007]
Training PASS
DRAM PHY training for 400MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x0000000d]
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000002]
[PMU Major message = 0x00000001]
[PMU Major message = 0x000000fd]
[PMU Major message = 0x000000fe]
[PMU Major message = 0x00000004]
[PMU Major message = 0x00000003]
[PMU Major message = 0x00000009]
[PMU Major message = 0x00000007]
Training PASS
DRAM PHY training for 100MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x0000000d]
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000002]
[PMU Major message = 0x00000001]
[PMU Major message = 0x000000fd]
[PMU Major message = 0x000000fe]
[PMU Major message = 0x00000004]
[PMU Major message = 0x00000003]
[PMU Major message = 0x00000009]
[PMU Major message = 0x00000007]
Training PASS
DRAM PHY training for 4000MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000005]
[PMU Major message = 0x00000005]
[PMU Major message = 0x00000006]
[PMU Major message = 0x00000006]
[PMU Major message = 0x00000007]
Training PASS
DDRINFO: ddrphy config done
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
>>SPL: board_init_r()
using memory lx-lx for malloc()
Normal Boot
Trying to boot from MMC1
clock is disabled (0Hz)
clock is enabled (400000Hz)
clock is enabled (400000Hz)
clock is enabled (50000000Hz)
spl: mmc boot mode: raw
spl_start_uboot retval :0 1:set define fault
load FDT file to RAM
hdr read sector ebf584, count=1
entry mmc_load_legacy function
SPL: payload image:                     Linux kernel load addr: 0x4047ffc0 size: 28013120
read d5ba sectors from 0xebf584 to 0x4047ffc0
ATF:read 0x60 sectors from 0xECDF80 to 0x970000
FDT-args:read 3d sectors from ebf520 to 43000000
Jumping to atf then linux
NOTICE:  BL31: v2.2(release):
NOTICE:  BL31: Built : 03:43:09, Apr 18 2023
[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.4.70 (mengfei@ubuntu2004-17) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Fri Apr 7 17:08:53 HKT 2023
[    0.000000] Machine model: NXP i.MX8MPlus LPDDR4 EVK board
[    0.000000] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
[    0.000000] printk: bootconsole [ec_imx6q0] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 320 MiB at 0x00000000ec000000
[    0.000000] NUMA: No NUMA configuration found
[    0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000001bfffffff]
[    0.000000] NUMA: NODE_DATA [mem 0x1bf3d6500-0x1bf3d7fff]
[    0.000000] Zone ranges:
[    0.000000]   DMA32    [mem 0x0000000040000000-0x00000000ffffffff]
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000001bfffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000040000000-0x00000001bfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000001bfffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] percpu: Embedded 24 pages/cpu s58904 r8192 d31208 u98304
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1548288
[    0.000000] Policy zone: Normal
[    0.000000] Kernel command line: console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200
[    0.000000] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
[    0.000000] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: mapped [mem 0xe8000000-0xec000000] (64MB)
[    0.000000] Memory: 5745992K/6291456K available (16636K kernel code, 1244K rwdata, 6556K rodata, 2880K init, 1017K bss, 217784K reserved, 327680K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[    0.000000]  Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 160 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: no VLPI support, no direct LPI support
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[    0.000000] ITS: No ITS available, not enabling LPIs
[    0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x44c with crng_init=0
[    0.000000] irq: no irq domain found for gpc@303a0000 !
[    0.000000] irq: no irq domain found for gpc@303a0000 !
[    0.000000] irq: no irq domain found for gpc@303a0000 !
[    0.000000] irq: no irq domain found for gpc@303a0000 !
[    0.000000] arch_timer: No interrupt available, giving up
[    0.000000] Failed to initialize '/timer': -22
[    0.000000] irq: no irq domain found for gpc@303a0000 !
[    0.000000] Failed to map interrupt for /soc@0/bus@30400000/timer@306a0000
[    0.000000] Failed to initialize '/soc@0/bus@30400000/timer@306a0000': -22
[    0.000000] timer_probe: no matching timers found
[    0.000000] Console: colour dummy device 80x25
[    0.000000] sched_clock: 64 bits at 250 Hz, resolution 4000000ns, wraps every 9007199254000000ns
[    0.000000] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[    0.000000] pid_max: default: 32768 minimum: 301
[    0.000000] LSM: Security Framework initializing
[    0.000000] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.000000] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.000000] ASID allocator initialised with 32768 entries
[    0.000000] rcu: Hierarchical SRCU implementation.
[    0.000000] EFI services will not be available.
[    0.000000] smp: Bringing up secondary CPUs ...
[    0.000000] Detected VIPT I-cache on CPU1
[    0.000000] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[    0.000000] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.000000] Detected VIPT I-cache on CPU2
[    0.000000] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[    0.000000] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.000000] Detected VIPT I-cache on CPU3
[    0.000000] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[    0.000000] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.000000] smp: Brought up 1 node, 4 CPUs
[    0.000000] SMP: Total of 4 processors activated.
[    0.000000] CPU features: detected: 32-bit EL0 Support
[    0.000000] CPU features: detected: CRC32 instructions
[    0.000000] CPU: All CPU(s) started at EL2
[    0.000000] alternatives: patching kernel code
[    0.000000] devtmpfs: initialized
[    0.000000] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.000000] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.000000] pinctrl core: initialized pinctrl subsystem
[    0.000000] DMI not present or invalid.
[    0.000000] NET: Registered protocol family 16
[    0.000000] DMA: preallocated 256 KiB pool for atomic allocations
[    0.000000] audit: initializing netlink subsys (disabled)
[    0.000000] audit: type=2000 audit(0.000:1): state=initialized audit_enabled=0 res=1
[    0.000000] cpuidle: using governor menu
[    0.000000] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.000000] Serial: AMBA PL011 UART driver
[    0.000000] imx mu driver is registered.
[    0.000000] imx rpmsg driver is registered.
[    0.000000] imx8mp-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[    0.000000] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.000000] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.000000] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.000000] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    0.000000] cryptd: max_cpu_qlen set to 1000
[    0.000000] ACPI: Interpreter disabled.
[    0.000000] iommu: Default domain type: Translated 
[    0.000000] vgaarb: loaded
[    0.000000] SCSI subsystem initialized
[    0.000000] usbcore: registered new interface driver usbfs
[    0.000000] usbcore: registered new interface driver hub
[    0.000000] usbcore: registered new device driver usb
[    0.000000] imx-i2c 30a20000.i2c: can't get irq number
[    0.000000] imx-i2c 30a30000.i2c: can't get irq number
[    0.000000] imx-i2c 30a40000.i2c: can't get irq number
[    0.000000] mc: Linux media interface: v0.10
[    0.000000] videodev: Linux video capture interface: v2.00
[    0.000000] pps_core: LinuxPPS API ver. 1 registered
[    0.000000] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[    0.000000] PTP clock support registered
[    0.000000] EDAC MC: Ver: 3.0.0
[    0.000000] No BMan portals available!
[    0.000000] QMan: Allocated lookup table at (____ptrval____), entry count 65537
[    0.000000] No QMan portals available!
[    0.000000] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[    0.000000] FPGA manager framework
[    0.000000] Advanced Linux Sound Architecture Driver Initialized.
[    0.000000] Bluetooth: Core ver 2.22
[    0.000000] NET: Registered protocol family 31
[    0.000000] Bluetooth: HCI device and connection manager initialized
[    0.000000] Bluetooth: HCI socket layer initialized
[    0.000000] Bluetooth: L2CAP socket layer initialized
[    0.000000] Bluetooth: SCO socket layer initialized
[    0.000000] VFS: Disk quotas dquot_6.6.0
[    0.000000] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.000000] pnp: PnP ACPI: disabled
[    0.000000] thermal_sys: Registered thermal governor 'step_wise'
[    0.000000] thermal_sys: Registered thermal governor 'power_allocator'
[    0.000000] NET: Registered protocol family 2
[    0.000000] tcp_listen_portaddr_hash hash table entries: 4096 (order: 4, 65536 bytes, linear)
[    0.000000] TCP established hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.000000] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes, linear)
[    0.000000] TCP: Hash tables configured (established 65536 bind 65536)
[    0.000000] UDP hash table entries: 4096 (order: 5, 131072 bytes, linear)
[    0.000000] UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes, linear)
[    0.000000] NET: Registered protocol family 1
[    0.000000] RPC: Registered named UNIX socket transport module.
[    0.000000] RPC: Registered udp transport module.
[    0.000000] RPC: Registered tcp transport module.
[    0.000000] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.000000] PCI: CLS 0 bytes, default 64
[    0.000000] kvm [1]: IPA Size Limit: 40bits
[    0.000000] kvm [1]: GICv3: no GICV resource entry
[    0.000000] kvm [1]: disabling GICv2 emulation
[    0.000000] kvm [1]: GIC system register CPU interface enabled
[    0.000000] kvm [1]: vgic interrupt IRQ1
[    0.000000] kvm [1]: kvm_arch_timer: uninitialized timecounter
[    0.000000] Initialise system trusted keyrings
[    0.000000] workingset: timestamp_bits=44 max_order=21 bucket_order=0
[    0.000000] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.000000] NFS: Registering the id_resolver key type
[    0.000000] Key type id_resolver registered
[    0.000000] Key type id_legacy registered
[    0.000000] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.000000] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    0.000000] 9p: Installing v9fs 9p2000 file system support
[    0.000000] Key type asymmetric registered
[    0.000000] Asymmetric key parser 'x509' registered
[    0.000000] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.000000] io scheduler mq-deadline registered
[    0.000000] io scheduler kyber registered
[    0.000000] imx8mq-usb-phy 381f0040.usb-phy: failed to get imx8mq usb phy clock
[    0.000000] imx8mq-usb-phy: probe of 381f0040.usb-phy failed with error -2
[    0.000000] imx8mq-usb-phy 382f0040.usb-phy: failed to get imx8mq usb phy clock
[    0.000000] imx8mq-usb-phy: probe of 382f0040.usb-phy failed with error -2
[    0.000000] EINJ: ACPI disabled.
[    0.000000] i.MX8MP clock driver probe done
[    0.000000] mxs-dma 33000000.dma-apbh: initialized
[    0.000000] Bus freq driver module loaded
[    0.000000] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.000000] imx-uart 30890000.serial: failed to request irq: -22
[    0.000000] imx-uart: probe of 30890000.serial failed with error -22
[    0.000000] imx-lcdifv3 32e80000.lcd-controller: No irq get
[    0.000000] loop: module loaded
[    0.000000] imx ahci driver is registered.
[    0.000000] libphy: Fixed MDIO Bus: probed
[    0.000000] tun: Universal TUN/TAP device driver, 1.6
[    0.000000] thunder_xcv, ver 1.0
[    0.000000] thunder_bgx, ver 1.0
[    0.000000] nicpf, ver 1.0
[    0.000000] pps pps0: new PPS source ptp0
[    0.000000] fec 30be0000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[    0.000000] fec 30be0000.ethernet: Using random MAC address: b6:a7:7b:fd:49:54
[    0.000000] Freescale FM module, FMD API version 21.1.0
[    0.000000] Freescale FM Ports module
[    0.000000] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[    0.000000] fsl_dpa: FSL DPAA Ethernet driver
[    0.000000] fsl_advanced: FSL DPAA Advanced drivers:
[    0.000000] fsl_proxy: FSL DPAA Proxy initialization driver
[    0.000000] fsl_oh: FSL FMan Offline Parsing port driver
[    0.000000] hclge is initializing
[    0.000000] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[    0.000000] hns3: Copyright (c) 2017 Huawei Corporation.
[    0.000000] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[    0.000000] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    0.000000] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[    0.000000] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    0.000000] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[    0.000000] igb: Copyright (c) 2007-2014 Intel Corporation.
[    0.000000] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[    0.000000] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.000000] sky2: driver version 1.30
[    0.000000] VFIO - User Level meta-driver version: 0.3
[    0.000000] dwc3 38100000.usb: Failed to get clk 'ref': -2
[    0.000000] dwc3 38200000.usb: Failed to get clk 'ref': -2
[    0.000000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    0.000000] ehci-pci: EHCI PCI platform driver
[    0.000000] ehci-platform: EHCI generic platform driver
[    0.000000] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[    0.000000] ohci-pci: OHCI PCI platform driver
[    0.000000] ohci-platform: OHCI generic platform driver
[    0.000000] usbcore: registered new interface driver uas
[    0.000000] usbcore: registered new interface driver usb-storage
[    0.000000] usbcore: registered new interface driver usbserial_generic
[    0.000000] usbserial: USB Serial support registered for generic
[    0.000000] usbcore: registered new interface driver ftdi_sio
[    0.000000] usbserial: USB Serial support registered for FTDI USB Serial Device
[    0.000000] usbcore: registered new interface driver usb_serial_simple
[    0.000000] usbserial: USB Serial support registered for carelink
[    0.000000] usbserial: USB Serial support registered for zio
[    0.000000] usbserial: USB Serial support registered for funsoft
[    0.000000] usbserial: USB Serial support registered for flashloader
[    0.000000] usbserial: USB Serial support registered for google
[    0.000000] usbserial: USB Serial support registered for libtransistor
[    0.000000] usbserial: USB Serial support registered for vivopay
[    0.000000] usbserial: USB Serial support registered for moto_modem
[    0.000000] usbserial: USB Serial support registered for motorola_tetra
[    0.000000] usbserial: USB Serial support registered for novatel_gps
[    0.000000] usbserial: USB Serial support registered for hp4x
[    0.000000] usbserial: USB Serial support registered for suunto
[    0.000000] usbserial: USB Serial support registered for siemens_mpi
[    0.000000] usbcore: registered new interface driver usb_ehset_test
[    0.000000] snvs_pwrkey: probe of 30370000.snvs:snvs-powerkey failed with error -22
[    0.000000] i2c /dev entries driver

 

 

タグ(2)
0 件の賞賛
返信
1 解決策
3,149件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @mengfei ,

 
I hope you are doing well.
 

 

NXP Yocto BSP does not support Falcon mode by default.
 
AN13709 has Falcon boot mode steps only for SD card.
 
Does Falcon mode support boot from EMMC? 
=> It should support Falcon boot from eMMC
.
     As Falcon mode does not support uuu. one has to boot normal mode u-boot from an SD card to flash ATF and Falcon bootloader image to emmc.
 
If the previous error message is resolved, can I mark this case as close?

 

 
Thanks & Regards,
Sanket Parekh

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,184件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hi @mengfei ,
 
I hope you are doing well.
 
This issue could be due to the Device tree (FDT) not being loaded correctly or an incorrect device tree.
 
To enable FDT in Falcon mode,
One needs to prepare FDT for SPL using u-boot (non-falcon mode).
 
Please make sure to follow step 18. in 4.3 Implementation in Linux Boot Time Optimizations for i.MX8M Family
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信
3,164件の閲覧回数
mengfei
Contributor III
Hi,
Does Falcon mode support booting from EMMC? In the manual, it is now booting from TF card.
0 件の賞賛
返信
3,150件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @mengfei ,

 
I hope you are doing well.
 

 

NXP Yocto BSP does not support Falcon mode by default.
 
AN13709 has Falcon boot mode steps only for SD card.
 
Does Falcon mode support boot from EMMC? 
=> It should support Falcon boot from eMMC
.
     As Falcon mode does not support uuu. one has to boot normal mode u-boot from an SD card to flash ATF and Falcon bootloader image to emmc.
 
If the previous error message is resolved, can I mark this case as close?

 

 
Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信