I try to load some images from USB flash drive. When issuing usb start with the flash drive on to the first USB I get some following information:
U-Boot 2018.09-36904-gae57ffc-dirty (Dec 18 2018 - 23:00:37 +0100)
CPU: Freescale i.MX6ULL rev1.1 792 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 49C
Reset cause: POR
Model: SomLabs i.MX6 ULL Visionsom
Board: SomLabs visionsom 6ull
DRAM: 512 MiB
NAND: 512 MiB
Loading Environment from NAND... *** Warning - bad CRC, using default environmet
Video: 800x480x24
In: serial
Out: serial
Err: serial
Net: FEC0 [PRIME]
Warning: FEC0 (eth0) using random MAC address - 46:79:2e:d4:3f:03
Somlabs iMX6ULL # usb start
starting USB...
USB0: USB EHCI 1.00
USB1: USB EHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
scanning bus 1 for devices... EHCI timed out on TD - token=0x80008d80
USB device not accepting new address (error=22)
1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
Somlabs iMX6ULL #
I'm trying to find the solution on different forums but without success. Hardware is OK because on U-Boot from 2017.03 it works well. Here is a list what I'm trying
int gave_extra_time = 0;
...
if ((srb->sense_buf[2] == 0x02) &&
(srb->sense_buf[12] == 0x3a))
return -1;...
/* If the status is "Not Ready - becoming ready", give it
* more time. Linux issues a spinup command (once) and gives
* it 100 seconds. */
if (srb->sense_buf[2] == 0x02 && srb->sense_buf[12] == 0x04 &&
gave_extra_time == 0)
gave_extra_time = retries = 1000; /* Allow 10 seconds. */
...mdelay(100);
} while (retries--);
The problem is with disappearing power supply on USB. The flash drive blinks shortly and disabled at all then. Nothing helps so far. On U-Boot 2017.03 when I issue usb start, the flash drive blinks 2 times and LED in it start beam constantly. Of course, all USB flash drive operations working well.
U-Boot is available at GitHub - SoMLabs/somlabs-uboot-imx - branch 2018.09 if someone want's to check parameters.
Hi Michal
SoMLabs uboot is not supported by nxp and this may be posted on uboot mail list
supported software is described on nxp official software page
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------