i.mx6ul brownout voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx6ul brownout voltage

跳至解决方案
1,786 次查看
vale90
Contributor I

Hello,

We are using a Phytec SOM which includes i.mx6ul. 

We use supercapacitor at the 3.3V supply of the SOM module.
When mains power is OFF; voltage goes down slowly and it gots stuck at lower than 3V levels.
Problem is; it doesn't reboot after power is ON (3.3V) again!

Note: If voltage goes lower than 1V; it works fine after power is ON again.
Note-2: We tried supplying the SOM with an adjustable DC source-only and removed supercaps. Same thing happens. Issue is not related with supercaps. It is something where some voltage levels makes the SOM stuck.

We couldn't solve this blind zone.

We trying to set-up brownout but we couldn't reach enough information. Would brownout solve this issue?

Thanks for your help.

标签 (3)
0 项奖励
回复
1 解答
1,704 次查看
vale90
Contributor I

Thank you Yuri.

We found the problem was boot SD card itself.

Some SD cards cause this problem (stucks at some voltage levels).

We insterted a new one; it didn't create this problem.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,705 次查看
vale90
Contributor I

Thank you Yuri.

We found the problem was boot SD card itself.

Some SD cards cause this problem (stucks at some voltage levels).

We insterted a new one; it didn't create this problem.

0 项奖励
回复
1,746 次查看
Yuri
NXP Employee
NXP Employee

@vale90 
Hello,

   the problem here concerns residual voltage of i.MX pins. This 
violates i.MX power up sequence.
  On the EVK discharge circuits (controlled by signal DISCHG_EN) are applied 

https://www.nxp.com/webapp/Download?colCode=MCIMX6UL-EVK_DESIGNFILES

 

Regards,
Yuri.

0 项奖励
回复