i.mx6sx lcd driver for RGB spi interface portting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6sx lcd driver for RGB spi interface portting

1,068 Views
chenmeng
Contributor II

i.mx6sx android 6.0 for lcd driver,the lcd driver have a spi interface,but  platform lcd driver has not mach the driver,help,help. 

Labels (1)
0 Kudos
Reply
1 Reply

915 Views
igorpadykov
NXP Employee
NXP Employee

Hi chen

such spi lcds are not supported in nxp bsps, one can look at below guidelines

for developing custom lcd driver with spi interface

http://www.gossamer-threads.com/lists/linux/kernel/1004162
https://lwn.net/Articles/341660/
http://elinux.org/images/1/19/Passing_Time_With_SPI_Framebuffer_Driver.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply