Hello all,
I've made a custom board with i.mx6 solo and i'm encountering some problems to make it boot!
Powrers and clocks are ok, BOOT_CFG are 0/0 and USB SERIAL DOWNLOADER is correctly prompted when attached to pc!
Uploading trough USB is fine (just doing boot and jump) but nothing happens after "jump" on the console neither on several clock pins (that remains high pulled).
After had same situation with several u-boot images (precompiled from freescale and my own), I think that there is some problem on DDR3.
So I made a little u-boot image and I'm trying to load it to OCRAM (TEXT_BASE = 0x009077e0), but nothng is happening the same, so the problem must be elsewhere!
Can you help me to find a way to make it boot?
Really thanks!
Hi, were you able to change the DDR clock speed inside u-boot? If so can you shared how you did it?
thanks a lot
Pat
Please try memory test linked below, at least to check if codes can be loaded to i.MX6 system and run there.
Thank you,
I was able to start the board by scaling the DDR clock to 400Mhz, but booting from internal ram.
Booting from DDR3 was not successfull!
Now it's time to start the DDR stress tester, to find out the correct register to set to make it works!
Unfrotunatly it hangs here:
MX6DL opened.
HAB_TYPE: DEVELOP
Image loading...
download Image to IRAM OK
Re-open MX6x device.
Running DDR test..., press "ESC" key to exit.
Do you have any tips to make it start?
Hello,
Now the DDR test is running but it ends/hangs here:
Beginning stress test
loop: 1
DDR Freq: 327 MHz
t0.1: data is addr test
Address of failure: 0x10000000
Data was: 0xff000000
But pattern should match address
Any tips?
Thank you very much!