Dear,
I have compile i.mx6qpsabresd borad,
we want use the linux 3.10 version.
Please check the this problem. I think mirror site(www.rpm5.org) is not access.
1. L3.14.52_1.1.0_LINUX_DOCS reference
2. ubuntu 14.04.06 LTS
3. Freescale Yocto Project User's Guide.pdf
$ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev
$ sudo apt-get install libsdl1.2-dev xterm sed cvs subversion coreutils texi2html docbook-utils python-pysqlite2 help2man make gcc g++ desktop-file-utils libgl1-mesa-dev libglu1-mesa-dev mercurial autoconf automake groff curl lzop asciidoc
$ sudo apt-get install u-boot-tools
$ mkdir ~/bin
$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ git config --global user.name "Your Name"
$ git config --global user.email "Your Email"
$ git config --list
$ mkdir fsl-release-bsp
$ cd fsl-release-bsp
$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga
$ repo sync
$ DISTRO=fsl-imx-x11 MACHINE=imx6qpsabresd source fsl-setup-release.sh -b build-x11
$ bitbake fsl-image-gui
---------------------------------------------------------------------------------------------------------------------------------------------------------------
ERROR: Fetcher failure: Fetch command failed with exit code 4, output:
wget: unable to resolve host address 'www.rpm5.org'
ERROR: Function failed: Fetcher failure for URL: 'http://www.rpm5.org/files/rpm/rpm-5.4/rpm-5.4.14-0.20131024.src.rpm;extract=rpm-5.4.14.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/test/fsl-release-bsp/build-x11/tmp/work/x86_64-linux/rpm-native/5.4.14-r0/temp/log.do_fetch.19876
ERROR: Task 94 (virtual:native:/home/test/fsl-release-bsp/sources/poky/meta/recipes-devtools/rpm/rpm_5.4.14.bb, do_fetch) failed with exit code '1'
---------------------------------------------------------------------------------------------------------------------------------------------------------------
Is there a way to fix it?
BR
Hi yun
linux 3.10 version is outdated and not more supported, recommended to migrate
to latest versions described on i.MX Software | NXP
Also git.freescale.com is not more used, one can try to follow steps described in
sect.4 Yocto Project Setup attached Yocto Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------