Hello,
How to I configure directfb to enable GPU acceleration of blitting and compositing operations?
Thanks,
Chuck
解決済! 解決策の投稿を見る。
Freescale i.MX6 BSP by default enables the DirectFB 1.4.0 GPU acceleration. To makesure, check the $(ROOTFS)/usr/lib/directfb-1.4-0/gfxdrivers/libdirectfb_gal.so is present and run df_dok benchmark application from DirectFB-examples to see the difference.
Freescale i.MX6 BSP by default enables the DirectFB 1.4.0 GPU acceleration. To makesure, check the $(ROOTFS)/usr/lib/directfb-1.4-0/gfxdrivers/libdirectfb_gal.so is present and run df_dok benchmark application from DirectFB-examples to see the difference.
Hello
I use the freescale directfb-1.7-4/gfxdrivers/libdirectfb_gal.so, and I also put it in the path of $(ROOTFS)/usr/lib/directfb-1.7-4/gfxdrivers/libdirectfb_gal.so,when I execute ./df_dok --accelonly,there is not picture on the screen, and the start infomation of DirectFB-example-1.2.0 is " Directfb/Graphics: Generic Sofeware Rasteriser 0.7 (directfb.org) ", I know it dosen't use the gpu of Vivante. When I execute ./df_dok, there are pictures on the screen.
How can I enable the gpu accelration of Vivante ?
I see a Netizen enable the directfb gpu acceleration, and the start infomation of DirectFB as follows :
"DirectFB/Graphics: Vivante unknown chip model 1.0 (Vivante)"
Where is the wrong ? Waiting for help!
Thank you!
Does the same library works for DirectFB v 1.6.0 ?
I use project yocto with version dylan, use the directfb v1.6.1 also, so....
Does the same library works for DirectFB v 1.6.1 ?
Yes it does work, even with directfb-1.6.3, but you have to make some link to make libdirectfb_gal.so workable :
ln -s /usr/lib/libdirectfb-1.6.so.0.3.0 /usr/lib/libdirectfb-1.4.so.0
ln -s /usr/lib/directfb-1.4-0/gfxdrivers /usr/lib/directfb-1.6-0/
But it does not work with directfb-1.7.0 :smileycry:
Is there an answer to this question?