Dear Freescale Engineer,
Resolution is set to 1920 X 1080, and we display a window desktop picture via HDMI to projector panasonic PT-BX410C.
We found that some lines in the corner of the picture are lost.
Please check the picture attached.
Other panasonic projector PT-UX333C doesn't has this problem.
Best regards,
Terry
Hi Terry,
Have you checked the image options of your projector? Some projectors as well as TVs have the option of adjust the image size/aspect ratio, for example 4x3, 16x9, stretched, full, and some times, part of the image is outside of the screen area, so, it is required to manually change the image option for fitting the screen (and it is independent of the resolution).
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------