i.mx6q HDMI output to projector panasonic PT-BX410C lines lost

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6q HDMI output to projector panasonic PT-BX410C lines lost

644 Views
terrytan
Contributor I

Dear Freescale Engineer,

Resolution is set to 1920 X 1080, and we display a window desktop picture via HDMI to projector panasonic PT-BX410C.

We found that some lines in the corner of the picture are lost.

Please check the picture attached.

Other panasonic projector PT-UX333C doesn't has this problem.

Best regards,

Terry无标题.jpg

Labels (4)
0 Kudos
Reply
1 Reply

564 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Terry,

Have you checked the image options of your projector? Some projectors as well as TVs have the option of adjust the image size/aspect ratio, for example 4x3, 16x9, stretched, full, and some times, part of the image is outside of the screen area, so, it is required to manually change the image option for fitting the screen (and it is independent of the resolution).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply