Hello,
I am using IMX6DL SABRE AUTO board and using android 8 BSP file was loaded.
To perform the ping test i have installed "Termux" app in android..I have connected PC to IMX6 board via ethernet cable to do ping test (point to point communication). PC can able to ping the IMX6 board but board can't able to ping the PC ip.I am getting "Network unavailable" error from the IMX6 board. Could you pls support. But i can able to connect a internet via ethernet cable from my router or other device.
Hello @B_Prabhu
I hope you are doing well.
->Please try to bring up the eth0 interface with the below-given command.
ifconfig <ethernet_interface> up
->Please also make sure to check the connection is properly made.
->Please check with the below-given command.
ping -I eth0 8.8.8.8
I hope this will work.
Thanks & Regards,
Sanket Parekh