i.mx6ULL USB Hardware Clarification and USB Detection.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6ULL USB Hardware Clarification and USB Detection.

1,136 次查看
theevanvenugopa
Contributor II

Hi NXP team,

Am very sad to inform you that I didn't get a response to previous emails.

Expecting your support for the following query.

1. In our custom board based on i.mx6ULL, we are only using the board only in USB device mode. For this, the Vbus(in our case it is USB_VBUS_iMX) voltage is necessary to connect to the i.MX's T12 pin??????(from HDG document I came to know that VBUS has no part in Power up sequence)

pastedImage_1.png

2. In the NXP EVK, we found a circuit as below. May I know the necessity of the same(Related to concern No:1)?

pastedImage_2.png

3. USB Data transfer detection is possible in i.MX? If yes, please provide the necessary details for implementing the same.

3 回复数

759 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  please look at my comments below.

1.

  Any of USB_OTG1_VBUS or USB_OTG2_VBUS may be applied for the USB

module of i.MX 6ULL. Your scheme (for USB_OTG1) is correct.

2.

   Basically VBUS may be provided directly from the connector.

3.

   I have some doubt if USB Data transfer detection is possible without data line

analyzing.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

759 次查看
theevanvenugopa
Contributor II

YuriMuhin_ng‌ Thank you for the support. 

At power-up sequence time, is that okay if VBUS reaches i.mx before DCDC_3V3? Also in the absence of DCDC_3V3(Power switch is OFF), Whether the presence of VBUS harms the IC?

0 项奖励

759 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  This already has been discussed.

https://community.nxp.com/message/966176 

Regards,

Yuri.

0 项奖励