i.mx6UL Qt widgets and applications

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6UL Qt widgets and applications

2,053 次查看
gokhansahin
Contributor III

Hi everyone, I have a question, think to use i.mx6UL or ULL in my project is HMI. 

However, yocto user guide in yocto-L4.1.15_2.0.0 says that;

Builds an opensource Qt 5 image. These images are onlysupported for i.MX SoC with hardware graphics. They arenot supported on the i.MX 6UltraLite, i.MX 6UltraLiteLite,and i.MX 7Dual.

What does it mean? Is it mean that I can not use it for Qt project? I'm quite confused.

Can I use all of the qt widgets such as multimedia for a camera, location for navigation etc. if I can use it?

标签 (1)
标记 (1)
3 回复数

1,470 次查看
joanxie
NXP TechSupport
NXP TechSupport

because this image is for e GPU(Graphics Processing Unit), mx6ul and mx7d don't have it.

1,470 次查看
gokhansahin
Contributor III

So, What should I do If I want to run Qt application in it? Is it possible with it?

0 项奖励
回复

1,470 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, you can follow the setup as below document:

https://community.nxp.com/docs/DOC-333580 

0 项奖励
回复