Hi,
on a custom board I see that VDD_PU cap is cycling on and off and wonder if that behavior is expected?
Running Linux 4.9.11.ga.
It cycles in periods of 1 to 1.5s when running a QT app with eglfs. When not running the app it stays off (~0.20V)
Looking at the PMU_REG_CORE with devregs the VDD_PU bit-field (REG1_TARG) toggles as well, between 00 and 26 (1175mV), e.g.
0x020c8140 =0x004c0012
0x020c8140 =0x004c2612
Using internal LDOs, no PMIC. SOC_IN supplied by 1.38V fixed regulator.
Is this behavior expected, and is it managed like this?
Hi ThomasG1z
yes this is correct behavior, as nxp linux turns off VDD_PU_CAP
when vpu/gpu modules are not used, one can look on Figure 51-1. Power system
overview i.MX6SDL Reference Manual
http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------