i.mx6 yocto cross compiler on u-boot spinor problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6 yocto cross compiler on u-boot spinor problem

1,184 次查看
eric_lee1
Contributor II

My custom board was running u-boot v2014.04 and Linux kernel 3.14.28. It is just fine. Lately, I upgraded to u-boot v2015.04 and linux kernel 4.1.15 that officially released from NXP. Everything is fine as expected. When using newer u-boot and kernel, I uses Linaro gcc-linaro-4.9-2015.05 cross compiler.

Then I started to working on Yocto build for newer kernel and u-boot (It was fine for u-boot v2014.04 and linux 3.14.28 yocto build). I found that the u-boot can only boot up from SD card. When boot up from spi nor flash, it will stop at

----

U-Boot 2015.04+fslc+g85a6a75 (Apr 12 2016 - 00:36:35)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 32 C

Reset cause: POR

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to HDMI

Display: HDMI (640x480)

(stop here)

---

Then I went to my yocto u-boot source directory at tmp/work/imx6q1gsmarc-poky-linux-gnueabi/u-boot-smarcfimx6/2015.04-smarcfimx6-r0+gitrAUTOINC+85a6a75394/git

And manually point to my cross compiler to Linaro gcc-linaro-4.9-2015.05 and manually build u-boot inside this directory. I can boot up from SPI NOR flash. I believe that the NXP new yocto release has this bug. When using arm-poky-linux-gnueabi- cross compiler to compile u-boot v2015.04, it cannot boot up from SPI flash.

May I know how to fix it from Yocto build?

-Eric

标签 (4)
0 项奖励
回复
1 回复

905 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  According to section  5.5 (U-Boot configuration) of 'Freescale_Yocto_Project_User's_Guide.pdf' :

"U-Boot configurations are defined in the main machine configuration file. The configuration is specified
by using the UBOOT_CONFIG settings. This requires setting UBOOT_CONFIG in local.conf.

Otherwise, the U-Boot build uses SD boot by default."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复