i.mx6-sabresd minipcie

cancel
Showing results for 
Search instead for 
Did you mean: 

i.mx6-sabresd minipcie

146 Views
strive
Contributor I

Dear  Expert:

I use the i.mx6-sabresd board to test pcie(host).

the linux version:L3.14.52,I have include the PCIe driver through bitake linux-imx menuconfig.

But I can not measure any clock in CLK1_N and CLK1_P.

pastedImage_1.png

in command window, input lspci -t ,it will show

-[0000:00]-

So could you tell me how i can configurate when i use the i.mx6 pcie(host)?

thanks for your support.

Labels (1)
0 Kudos
1 Reply

41 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Tom

one can try to test pcie in uboot, please check #define CONFIG_CMD_PCI in

uboot/include/configs/mx6sabresd.h

uboot-imx.git - Freescale i.MX u-boot Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos