i.mx6 quad CPU on EDM SOM module. Constantly hangs after system start.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6 quad CPU on EDM SOM module. Constantly hangs after system start.

1,373件の閲覧回数
sergeym
Contributor I

Hello

I've got this SOM module http://www.technexion.com/products/edm/edm-som/edm1-cf-imx6 with i.MX quad processor installed on the fairy board http://www.technexion.com/products/edm/edm-carrier-boards/edm1-fairy

It has factory installed linux images in flash memory. I tried Ubuntu 12.04 first but it hangs after I start browsing via Firefox. Sometimes it hangs when in terminal but it's pretty rare.

I've tried Yocto, but it hangs too when I open some app with graphics.

Here is some ubuntu logs after reboot:

https://drive.google.com/file/d/0B4r-ZIonbU1vQ2dLZDB4SVNtZms/view?usp=sharing

Sorry, I'm a newbie Linux user.

With best regards, Sergey

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,092件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Do you flash the image following the instructions of the  User Guide :

http://www.technexion.com/images/downloads/edm/modules/edm1-cf-imx6/edm1-cf-imx6-userguide-091.pdf

What about the heatsink, do you added? do you think you can share more details,  besides the log,  like power supply, or have you contact Technexion?

0 件の賞賛
返信

1,092件の閲覧回数
sergeym
Contributor I

@jamesbone

Sure, I've followed the instructions.

Yup, I added a custom heatsink with thermal grease.

https://drive.google.com/file/d/0B4r-ZIonbU1va0hWYlg3aUc1LWc/view?usp=sharing

https://drive.google.com/file/d/0B4r-ZIonbU1vM2d5ZmYwVV8wNjQ/view?usp=sharing

I use power supply from TechNexion Fairy board http://www.technexion.com/images/downloads/edm/carrierboards/edm1-fairy/edm1-fairy-userguide-091.pdf

I've got an advice from TechNexion yesterday, but they're talking about possible overheat issue. Though this cooler is just warm.

0 件の賞賛
返信