Hi
We have developed board which uses SMARC-sAMX6i module from Kontron. In SSI bus we have MAX98357A PCM input class D audio amplifier which takes either I^2S or TDM data
and acts as slave for SSI bus. We are using kernel 3.14 so which are the stpes to get SSI bus and maxim working?
- dts configure settings so we can write raw data to /dev/i2s device
or
- Do we need create ALSA driver for that or is there driver already in kernel which have to activate in device tree?
- Something else ?
Thanks,
Ari Savolainen
解決済! 解決策の投稿を見る。
Hi Ari
one can follow steps described in attached Porting Guide
Chapter 8 Porting Audio Codecs to a Custom Board
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI
Now sound is working :smileyhappy:
Problem was that original qcom,storm driver from kernel 4.4 tree did not adjust i2S bus to master mode and probably audmux was not set correctly. Many thanks to igorpadykov for tips and suggestions.
Problem was solved taking max98357a driver from kernel 4.4 and using imx-si476x.c driver file as example for codec link driver.
Ari
hei,
Would you Ari be willing to share the code you have for MAX98357a? I quess that MAX98357a driver is the one directly from the existing tree but the qcom storm driver and needed bindings for device tree and build instructions are what I need.
I am facing same issue now and would be thankful if I could share your implementation.
br AriS
Hi Ari Sinisalo
Check attached zip file. There you can find three files. Files are
- sound.dts (This is device tree source which combines actual sound card driver and codec. Also sets SSI bus to master mode)
- imx-pt10ex.c (sound card driver)
- max98357a.c (codec)
We are using modified kernel 3.14.28 and these files are extracted directly from kernel tree. You have to also create kernel Makefile changes accordingly
Best Regards
Ari Savolainen
I tried to follow your instructions, I am using the same amplifier but its on the imx7, this is the error I get:
[ 2.043559] imx-pt10ex-audio sound1: imx_pt10ex2_probe called.
[ 2.050896] imx-pt10ex-audio sound1: int_port set to value 1
[ 2.057974] imx-pt10ex-audio sound1: ext-port set to value 3
[ 2.065091] imx-pt10ex-audio sound1: Platform device disabled. i2c not used by sound card
[ 2.075958] imx-pt10ex-audio sound1: ASoC: CODEC DAI max98357a not registered
[ 2.084525] imx-pt10ex-audio sound1: Failed to register card: -517
My device tree file looks like this now:
<p>/ {
codec_mono: max98357a@0 {
compatible = "maxim,max98357a";
#sound-dai-cells = <0>;
};
sound1 {
compatible = "pt,pt10ex-audio";
pt,model = "pt10ex";
ssi-controller = <&sai2>;
codec = <&codec_mono>;
};
};
&sai2 {
fsl,mode = "i2s-master";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai2>;
assigned-clocks = <&clks IMX7D_SAI2_ROOT_SRC>,
<&clks IMX7D_SAI2_ROOT_CLK>;
assigned-clock-parents = <&clks IMX7D_PLL_AUDIO_POST_DIV>;
assigned-clock-rates = <0>, <36864000>;
status = "okay";
};</p>
Do you have any ideas?
It seems that max98357a codec is not loaded. Check that driver is built with kernel or has built as module
Hi
We are struggling with this case still. aplay -D hw:0,0 <some file> works fine but there is no sound. Data is not sended to SSI bus. That is verified with oscilloscope from LRCLK, BCLK and SDATA pins.
ALSA drivers is debug traced so they seems to work OK, so fsl_ssi / AUDMUX is probable not working. Is there some sample DTS settings for SSI1 as master config available somewhere so we can check our own config?
Hi Ari
one can follow steps described in attached Porting Guide
Chapter 8 Porting Audio Codecs to a Custom Board
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
igorpadykov kirjoitti:
Hi Ari
one can follow steps described in attached Porting Guide
Chapter 8 Porting Audio Codecs to a Custom Board
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I found drivers from kernel 4.4 tree for Maxim 98357a , so now I have alsa device in kernel. Files which was adapted and edited was max98357a.c and storm.c
So now we have
I created dts bindings also so now there is alsa device in /proc/asound/cards
900001:~# cat /proc/asound/cards
0 [pt10ex ]: pt10ex - pt10ex
pt10ex
1 [imxhdmisoc ]: imx-hdmi-soc - imx-hdmi-soc
imx-hdmi-soc
And drivers gets loaded normally
900001:~# dmesg | grep 'max\|pt10ex\|ssi'
imx-sdma 20ec000.sdma: no iram assigned, using external mem
max98357a:max98357a_platform_probe
fsl_ssi:fsl_ssi_probe OK
pt10ex-audio:pt10ex_parse_of OK
max98357a:max98357a_codec_probe OK
pt10ex-audio sound.29: HiFi <-> 2028000.ssi mapping ok
pt10ex-audio:pt10ex_platform_probe OK, ret=0, name=pt10ex, Long name=(null), dev->init_name=(null)
#0: pt10ex
pt10ex-audio: pt10ex_ops_hw_params OK
For some reason there is no sound when I try to test card.
900001:~# aplay -f S16_LE -Dhw:0,0 /dev/urandom
Playing raw data '/dev/urandom' : Signed 16 bit Little Endian, Rate 8000 Hz, Mono
Aborted by signal Interrupt...
Can I debug trace SSI bus somehow in kernel side so I can find that data is sended to max98357a codec?
Ari
also one can try unit-test:
mxc_ssi_test/
http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/
or Chapter 28 attached Linux Manual, sect.28.5 Unit Test
Best regards
igor
Hi
One more question:
Because Maxim 98357a codec acts as slave for SSI do I have to congigure SSI1 somehow? We have have only activated SSI from device tree.
Ari
Thanks for your quick reply. Is there any quick way to test new hardware before developing driver? For example
cat /dev/urandom > /dev/SSI1
or something like that?
Hi Ari,
If you want to test the MAX98357A you can order a Evaluation Kit from our website
MAX98357DEV#WLP Evaluation System for the MAX98357A and MAX98357B (WLP) - Maxim
Otherwise, you can generate a I2S or TDM sample signal from you microprocessor unit and make sure you follow the datasheet voltage requirements for the MAX98357A PCM Input Class D Audio Power Amplifiers - Maxim
I hope this helps!
- Felipe
Hi Felipe
We have used your evaluation kit already and that is OK. Max98357A takes i2s or TDM data and question is how can we offer it from Linux system.
aplay /dev/urandom
You cannot use aplay /dev/urandom if you do not have alsa driver yet.