i.mx6 dual/quad EIM interface bandwidth

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 dual/quad EIM interface bandwidth

1,074 Views
technect
Contributor II

I am considering using EIM I/F between i.mx6 and FPGA, I want to know the max bandwidth of EIM I/F. Is there the result of measured speed?

Labels (1)
0 Kudos
Reply
1 Reply

782 Views
igorpadykov
NXP Employee
NXP Employee

Hi Seung-Gon

I am not aware of such performance data, however

please look at considerations below regarding max bandwidth of EIM :

https://community.freescale.com/docs/DOC-103127

https://community.freescale.com/docs/DOC-106467

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply