i.mx6 can't connect with USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6 can't connect with USB

374件の閲覧回数
yun1405007
Contributor I

    Hi everybody:   According to the official manual,we design circuit again about  I.MX6 processor,now,we tested the board yestoday,But,

the board can't be recognised in USB.VDDCORE and VDDSOC is 1.4V, VDD_HIGH_IN and NSNVS are 3.0V.All supply voltages

are in line with  the official manual.There are nothing wrong in multiplexing I / O ports and power-up sequence,However,we alway can't connect with USB.To our strange,when VDDCORE and VDDSOC voltage at around 1.2V ,USB can be connected,but Loading image fails .

thanks

0 件の賞賛
1 返信

306件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could refer to section 3.11 “USB recommendations” of the “Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processo...” document and to section 3.4.1.2 “USB” of the application note AN3951 “i.MX Layout Recommendations”.

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛