i.mx6 VDD_HIGH_IN current drawn

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 VDD_HIGH_IN current drawn

Jump to solution
718 Views
mehmetertugafsi
Contributor II

In my custom i.mx6 board design, i m going to use LVDS and SATA which effects the current calculation of VDD_HIGH_IN as stated below. So base max current drawn is 125 mA as stated in datasheet, however i couldnt find any information regarding maximum current drawn from NVCC_LVDS_2P5 and SATA. There is typical current drawn from sata but not max. So how much current capability shall i allocate for VDD_HIGH_IN?

The note from the datasheet says:

"The actual maximum current drawn from VDD_HIGH_IN will be as shown plus any additional current drawn from the VDD_HIGH_CAP outputs, depending upon actual application configuration (for example, NVCC_LVDS_2P5, NVCC_MIPI, or HDMI, PCIe, and SATA VPH supplies)."

Labels (5)
0 Kudos
1 Solution
519 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mehmet

VDD_HIGH_IN requirements are described in Sabre schematic spf-27392 p.20

spf27392 p.20.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
520 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mehmet

VDD_HIGH_IN requirements are described in Sabre schematic spf-27392 p.20

spf27392 p.20.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

519 Views
mehmetertugafsi
Contributor II

Thank you..

0 Kudos