i.mx6 Solo DDR Stress Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 Solo DDR Stress Test

1,471 Views
srikittu34
Contributor II

HI All,

iam doing ddr3 stress test to imx6 solo board..here i am getting this error everytime..

 https://community.nxp.com/servlet/JiveServlet/downloadBody/94917-102-14-285076/I. 

https://community.nxp.com/servlet/JiveServlet/download/339795-1-419286/DDR_Stress_ 

loop: 1

DDR Freq: 396 MHz

t0.1:data is addr test

address of failure:0x30000000

data was:0x03000024

but pattern should match address

ddr nxp.PNG

please give me some guidance for how to run ddr stress test successfully..!

thanks & regards,

srikrishna

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,066 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 

   please check if Your PCB design satisfies recommendations of the  HW_Design_Checking_List_for_i.MX6DQP6DQ6SDL:

 

HW_Design_Checking_List_for_i.MX6DQP6DQ6SDL 

 

https://community.nxp.com/servlet/JiveServlet/downloadBody/93819-102-17-270033/HW_Design_Checking_Li... 

 

  In particular, use the sheet, named "MX6 DRAM Bus Length Check".

 

 

Have a great day,

Yuri

 ------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

1,066 Views
srikittu34
Contributor II

thank you @Yuri Muhin for giving such guidance..

again i am facing the same issue .,a small doubt on this that i.mx6 solo board stress test already done successfully before 4 months ..

so i'm trying to do again on this board is that will give the same result or i have to go with a new board..!

best regards,

srikrishna.

0 Kudos
Reply

1,066 Views
Yuri
NXP Employee
NXP Employee

Hello,

  perhaps it makes sense to perform memory calibration again and use its 

results in the initialization code.

Regards,

Yuri.