Display (color bit mapping is software configurable. When configuring display output pins,
the following should be taken into account.
1.
General scheme is shown on Figure 37-32 (Mapping scheme) of the i.MX6DQRM.
2.
From Table 37-25 (DC template's fields description) :
«The MAPPING field holds a pointer to a register holding 3 fields: MAPPING_PNTR_BYTE0_X,
MAPPING_PNTR_BYTE1_X, MAPPING_PNTR_BYTE2_X. This pointers point to sets of OFFSET and
MASK parameters that define the mapping scheme. MAPPING =0 means that mapping is disabled.»
3.
Section 37.4.7.5.1 (Bus Mapping Unit) describes the mapping feature in more details.
On the Figure 37-32 (Mapping scheme), microcode field MAPPING = 2.
That is, register IPUx_DC_MAP_CONF_1 should be used for configuring; please refer to section 37.5.336
[DC Mapping Configuration Register 1 (IPUx_DC_MAP_CONF_1)] of the Reference Manual.
As an example let we set :
MAPPING_PNTR_BYTE2_2 = 2
MAPPING_PNTR_BYTE1_2 = 1
MAPPING_PNTR_BYTE0_2 = 0
then
IPUx_DC_MAP_CONF_15 register should be set as following :
(section 37.5.350 DC Mapping Configuration Register 15 (IPUx_DC_MAP_CONF_15))
MD_OFFSET_1 = 0x0D ; MD_MASK_1 = 0xFC
MD_OFFSET_0 = 0x05 ; MD_MASK_0 = 0xFC
IPUx_DC_MAP_CONF_16 :
MD_OFFSET_2 = 0x16 ; MD_MASK_2 = 0xFC
4.
Please refer to Chapter 18 (Configuring the IPU Driver) of "iMX6_Firmware_Guide.pdf" in the Platform SDK.
https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab
5.
Please use i.MX6 Datasheet(s) to define typical IPU display output formats.
For example please take a look at section 4.11.10.4 (IPU Display Interface
Signal Mapping) of IMX6SDLCEC (Rev. 2.1, 05/2013).