I get the libfslmscodec-3.0.7.tar.gz and libfslmsparser-3.0.7.tar.gz package from Freescale.
But failed to play a wma file.
--------------
root@freescale ~$
root@freescale ~$ export GST_DEBUG=2
root@freescale ~$
root@freescale ~$
root@freescale ~$
root@freescale ~$ gplay /2205/001.wma
playbin2 is employed!
fsl_player_init(): Successfully initialize!
fsl_player_set_media_location(): filename=/2205/001.wma
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]Aiur: 3.0.7
Core: ASFPARSER_01.00.17 build on Jun 25 2013 10:17:36
mime: video/x-ms-asf
file: /usr/lib/imx-mm/parser/lib_asf_parser_arm11_elinux.so.3.1
Content Info:
URI:
file:///2205/001.wma
Idx File:
/root/.aiur/.2205.001.wma.aidx
Seekable : Yes
Size(byte): 93005
0:00:00.126050000 2769 0xd34c8 WARN aiurdemux aiurdemux.c:3676:aiurdemux_loop_state_header: Warning: API[getNumPro!
Movie Info:
Seekable : Yes
Live : No
Duration : 0:02:30.300000000
ReadMode : File
Track : 1
0:00:00.126615000 2769 0xd34c8 WARN aiurdemux aiurdemux.c:3060:aiurdemux_parse_audio: Unknown Audio code-type=0, s0
(<unknown>:2769): GStreamer-CRITICAL **: gst_tag_list_add: assertion `GST_IS_TAG_LIST (list)' failed
Track 00 [audio]: Disabled
Codec: 0, SubCodec: 0
0:00:00.126977000 2769 0xd34c8 WARN aiurdemux aiurdemux.c:4312:aiurdemux_pull_task: pausing task, reason error
0:00:00.127055667 2769 0xd34c8 WARN aiurdemux aiurdemux.c:4332:aiurdemux_pull_task:<aiurdemux0> error: streaming s2
state change failed from 2 to 4
try to play failed
0:00:00.128081000 2769 0x15700 WARN aiurdemux aiurdemux.c:1927:gst_aiurdemux_close_core: API[exportIndex] failed, 2
FSL_PLAYER_01.00_LINUX build on Aug 29 2014 10:45:16
[h]display the operation Help
[p]Play
[s]Stop
[e]Seek
[a]Pause when playing, play when paused
[v]Volume
[m]Switch to mute or not
[>]Play next file
[<]Play previous file
[r]Switch to repeated mode or not
[f]Set full screen or not
[z]resize the width and height
[t]Rotate
[c]Setting play rate
[i]Display the metadata
[x]eXit
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]
--------------
How can i fix the issue ?
Original Attachment has been moved to: 001.wma.zip
Solved! Go to Solution.
this file is wma voice file, mx6 couldnt support this, just support wma std pro lossless, not support voice
this file is wma voice file, mx6 couldnt support this, just support wma std pro lossless, not support voice
Thanks a lot !
I think it is not correct to say "mx6 couldn't support this". I guess you meant that the FSL audio codec package does not support it.
On Ubuntu I can play this file with no issues:
gst-launch-1.0 -v playbin uri=file:///home/fabio/Downloads/001.wma
thanks for your reminder, I mean the FSL special codec the customer used doesn't support this.