i.mx6 Failed to play wma file

cancel
Showing results for 
Search instead for 
Did you mean: 

i.mx6 Failed to play wma file

Jump to solution
869 Views
tongchunyang
Contributor III

I get the libfslmscodec-3.0.7.tar.gz and libfslmsparser-3.0.7.tar.gz package from Freescale.
But failed to play a wma file.


--------------
root@freescale ~$
root@freescale ~$ export GST_DEBUG=2
root@freescale ~$
root@freescale ~$
root@freescale ~$
root@freescale ~$ gplay /2205/001.wma
playbin2 is employed!
fsl_player_init(): Successfully initialize!
fsl_player_set_media_location(): filename=/2205/001.wma
[Stopped  ][Vol=01][00:00:00/00:00:00][fps:0]Aiur: 3.0.7
Core: ASFPARSER_01.00.17  build on Jun 25 2013 10:17:36
  mime: video/x-ms-asf
  file: /usr/lib/imx-mm/parser/lib_asf_parser_arm11_elinux.so.3.1
Content Info:
        URI:
              file:///2205/001.wma
        Idx File:
              /root/.aiur/.2205.001.wma.aidx
        Seekable  : Yes
        Size(byte): 93005

0:00:00.126050000  2769    0xd34c8 WARN               aiurdemux aiurdemux.c:3676:aiurdemux_loop_state_header: Warning: API[getNumPro!
Movie Info:
        Seekable  : Yes
        Live      : No
        Duration  : 0:02:30.300000000
        ReadMode  : File
        Track     : 1

0:00:00.126615000  2769    0xd34c8 WARN               aiurdemux aiurdemux.c:3060:aiurdemux_parse_audio: Unknown Audio code-type=0, s0

(<unknown>:2769): GStreamer-CRITICAL **: gst_tag_list_add: assertion `GST_IS_TAG_LIST (list)' failed
Track 00 [audio]: Disabled
        Codec: 0, SubCodec: 0
0:00:00.126977000  2769    0xd34c8 WARN               aiurdemux aiurdemux.c:4312:aiurdemux_pull_task: pausing task, reason error
0:00:00.127055667  2769    0xd34c8 WARN               aiurdemux aiurdemux.c:4332:aiurdemux_pull_task:<aiurdemux0> error: streaming s2
state change failed from 2 to 4
try to play failed
0:00:00.128081000  2769    0x15700 WARN               aiurdemux aiurdemux.c:1927:gst_aiurdemux_close_core: API[exportIndex] failed, 2

FSL_PLAYER_01.00_LINUX build on Aug 29 2014 10:45:16
        [h]display the operation Help
        [p]Play
        [s]Stop
        [e]Seek
        [a]Pause when playing, play when paused
        [v]Volume
        [m]Switch to mute or not
        [>]Play next file
        [<]Play previous file
        [r]Switch to repeated mode or not
        [f]Set full screen or not
        [z]resize the width and height
        [t]Rotate
        [c]Setting play rate
        [i]Display the metadata
        [x]eXit
[Stopped  ][Vol=01][00:00:00/00:00:00][fps:0]


--------------

How can i fix the issue ?

Original Attachment has been moved to: 001.wma.zip

Labels (2)
0 Kudos
1 Solution
208 Views
joanxie
NXP TechSupport
NXP TechSupport

this file is wma voice file, mx6 couldnt support this, just support wma std pro lossless, not support voice

View solution in original post

0 Kudos
4 Replies
209 Views
joanxie
NXP TechSupport
NXP TechSupport

this file is wma voice file, mx6 couldnt support this, just support wma std pro lossless, not support voice

View solution in original post

0 Kudos
208 Views
tongchunyang
Contributor III

Thanks a lot !

0 Kudos
208 Views
fabio_estevam
NXP Employee
NXP Employee

I think it is not correct to say "mx6 couldn't support this". I guess you meant that the FSL audio codec package does not support it.

On Ubuntu I can play this file with no issues:

gst-launch-1.0 -v playbin uri=file:///home/fabio/Downloads/001.wma

208 Views
joanxie
NXP TechSupport
NXP TechSupport

thanks for your reminder, I mean the FSL special codec the customer used doesn't support this.

0 Kudos