I have a car: Opel Insignia with a radio running on "i.MX 6 DL D3 Board, DTBID 30db, 896MB DRAM". Here is what's in the file (/ etc / issue):
"ADIT: inte-imx6_r3_e22-G3-MC0 mgc-imx6 Arm -
DISTRI: MGC_20140501 Spring-2014-05 -
Hotfix: 439
Architecture: mx6q - cortexa9-vfp-neon ".
Unfortunately, I'm not very good at Linux, but I hope you can help me. Is there a way through the USB drive to access the system to change files or add new ones?
Currently the system only allows USB with music content or videos.
I found information about "u-boot". Can that help me?
I have tried to connect a USB keyboard via the USB port, but unfortunately this is not recognized or approved.
If i can give you more informations or other discription so ask.
I have the Software which is installed on the board, if it helps someone to find "a possibility".
thk
Does the OS allow to run scripts from USB drive?
If yes you can pack the new files into archive and make a script that unpacks the files into their place.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I am not sure. It is possible to update via USB, or to update the navigation maps by updating, music and videos are also recognized. As I found out so far this happens over the "udev rules". if you could change the folder, it would certainly be possible to execute scripts.