i.mx6 CSI->IC->MEM gamma correction possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 CSI->IC->MEM gamma correction possible?

674 Views
davemcmordie
Contributor III

I see that gamma correction has been implemented in the image converter (IC) for display colour correction purposes.  Is it possible to use this same image converter functionality to perform gamma correction of an incoming CSI capture stream?  

If so, what changes would be needed to implement this?

Tags (3)
0 Kudos
1 Reply

485 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dave

one can look at examples in ips_csc.c in iMX6_Platform_SDK\sdk\drivers\ipu\test\ips_csc.c

swp-report/iMX6_Platform_SDK at master · backenklee/swp-report · GitHub 

https://community.freescale.com/docs/DOC-94961

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos