i.mx53qsb USB Error device descriptor read/64, error -71

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53qsb USB Error device descriptor read/64, error -71

3,225 Views
guohn
Contributor III

Dear all,

     I use i.mx53qsb to connect usb storage when start linux system. And sometimes occur error.

usb 1-1: device not accepting address 2, error -71

usb 1-1: new low speed USB device using fsl-ehci and address 3

usb 1-1: device not accepting address 3, error -71

usb 1-1: new low speed USB device using fsl-ehci and address 4

usb 1-1: device descriptor read/64, error -71

usb 1-1: device descriptor read/64, error -71

usb 1-1: new low speed USB device using fsl-ehci and address 5

usb 1-1: device descriptor read/64, error -71

usb 1-1: device descriptor read/64, error -71

hub 1-0:1.0: unable to enumerate USB device on port 1

     When start the linux system, sometimes can plug usb storage, and sometimes can't.

     What can cause this error?

Best regard


Labels (1)
0 Kudos
4 Replies

1,145 Views
raymondwang
Senior Contributor I

-71 means IO error, it seems usb port unstable ,maybe board issue or usb device issue.

You can retry with low speed usb device like usb mouse. If it works, usb port is unstable

for high speed. Then you can check your usb cable.

0 Kudos

1,145 Views
guohn
Contributor III

Thanks!

     I have two i.mx53qsb board. I try to test the two board, but the two board sometimes can occur the error.

0 Kudos

1,145 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi guo,

I have tested on my board, I haven't seen this issue. I think it's maybe the power problem on your hardware, would you please check?

Best Regards

Dan

0 Kudos

1,145 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi guo,

-71 means IO error, make sure usb mouse is connected properly.

Best Regards

Dan

0 Kudos