i.mx535的开发环境搭建

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx535的开发环境搭建

1,918 次查看
caifaguo
Contributor II

请问哪边可以下载到i.mx535的编译器

还有qt4.8.7的环境搭建的教程 急需

谢谢

标签 (1)
6 回复数

1,697 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using? The i.MX53 is old products, so no newest BSP update. The following thread will do help for you.

i.MX53 Multimedia Applications Processors 

https://community.nxp.com/docs/DOC-94123 

0 项奖励
回复

1,697 次查看
caifaguo
Contributor II

你们有i.mx535 qsb开发板的光盘吗?可以给我一份吗?非常感谢

0 项奖励
回复

1,697 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you want the BSP or Demo images?

0 项奖励
回复

1,697 次查看
caifaguo
Contributor II

I want the compilers and ltib now. I don`t howto build they.when I build them happen many errors.So I saw the data the i.mx535 qsb board dvd have the sdk(ubuntu 10.04 L2.6.35_11.09.01_ER_docs and so on). could you give the dvd data download url. 

many url of i.mx535 is lose.So I can`t find the data what I need.

thank you!

0 项奖励
回复

1,697 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,697 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

OK, I will share to you tomorrow.