i.mx53 quick start board + raspberry pi camera (ov5647 )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53 quick start board + raspberry pi camera (ov5647 )

680 Views
danielcogianu
Contributor I

Hello,

I bought a i.mx53 quick start board and I want to connect it to a raspberry pi camera. Did anyone try to do this?

I have not found any data about the raspberry pi camera connector pinout.

I am thinking to separate the ov5647  camera (which has a datasheet) from the raspberry pi module and to try to use it.

Can anyone help me with some advices?

Thank you

Labels (1)
0 Kudos
1 Reply

370 Views
SergioSolis
NXP Employee
NXP Employee

I haven't personally done that, but there is an expansion board for the QSB with the camera CSI port signals.

You might want to use that expansion board, it would definitely make things easier.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos