i.mx51 display driver has function Screen off?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx51 display driver has function Screen off?

跳至解决方案
1,653 次查看
oogata
Contributor I

Hi All!

I am working on i.mx51 customized board.

I am worried about LCD Burn-In. I would like to screen off.

Please tell me, In Windows CE 6.0 Freescale BSP, the Display Driver, or would have been implemented function screen off?

Thank you,

Ogata

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,466 次查看
jimmychan
NXP TechSupport
NXP TechSupport

"The DI and DC submodules of the IPUv3 are disabled.". It is means DI and DC ( the submodules in the IPUv3) disable, not the whole IPUv3 module disable.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,466 次查看
jimmychan
NXP TechSupport
NXP TechSupport

According to the i.MX51 WinCE6 BSP Reference manual 8.4.4.3  IOCTL_POWER_SET,

The display driver implements the IOCTL_POWER_SET IOCTL API with support for the D0 (Full On) and D4 (Off) power states. These states are handled in the following manner:

• D0—The display panel is enabled. The IPUv3 DI and DC modules are enabled to send data to thedisplay. If video is active, additional submodules may also be enabled to process and convert video data. If TV output mode is active, enable the TVE module and its clocks.

• D4—The DI and DC submodules of the IPUv3 are disabled. The display panel is disabled. If TV output mode was enabled, disable the TVE and its clocks.

Have you try this?

1,466 次查看
oogata
Contributor I

Thanks for your reply, jimmy.

I'll try "IOCTL_POWER_SET, D4".

I have heard that the cause of LCD-burn-in is long time displaying of same contents.

BSP Reference manual 8.4.4.3 ,wrote

   "The DI and DC submodules of the IPUv3 are disabled."

Are "the IPUv3 are disabled" mean that to stop the display ?

0 项奖励
回复
1,467 次查看
jimmychan
NXP TechSupport
NXP TechSupport

"The DI and DC submodules of the IPUv3 are disabled.". It is means DI and DC ( the submodules in the IPUv3) disable, not the whole IPUv3 module disable.

0 项奖励
回复