i.mx280 ethernet + nand

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx280 ethernet + nand

Jump to solution
1,826 Views
yar
Contributor III

Hello,

I am new in I.MX28x family MCU. I want to use NAND (GPMI) + ETHERNET (ENET) together.

I tried to test this configuration in Freescale IO Mux application. Application shows the presence of conflict (screenshot attached).

Whether correctly I understand that in I.MX280 it is impossible to use NAND + ETHERNET simultaneously?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,698 Views
VladanJovanovic
NXP Employee
NXP Employee

Typically you use only one or two NAND chips on designs, so with that you should be fine (GPMI_CE0N, GPMI_CE1N, GPMI_READY0, GPMI_READY1).

If you want to attach additional four NANDs, then yes, you will have some conflicts, but that is not a very typical design.

View solution in original post

0 Kudos
Reply
2 Replies
1,699 Views
VladanJovanovic
NXP Employee
NXP Employee

Typically you use only one or two NAND chips on designs, so with that you should be fine (GPMI_CE0N, GPMI_CE1N, GPMI_READY0, GPMI_READY1).

If you want to attach additional four NANDs, then yes, you will have some conflicts, but that is not a very typical design.

0 Kudos
Reply
1,698 Views
yar
Contributor III

Thanks for the detailed answer.

0 Kudos
Reply