Hi all, Qiang_FSL
I have a Winbond nor flash on my board, W25Q256. After seeing the site: How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s) I want to use the jffs2 too.
But when mounting jffs2 during kernel starting, I keep seeing lots of jffs2 error,
mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:00:34 UTC (34)
VFS: Mounted root (jffs2 filesystem) on device 31:1.
Freeing init memory: 176K
JFFS2 notice: (999) read_dnode: node CRC failed on dnode at 0x1be007c: read 0xb08d1054, calculated 0x8b624504
JFFS2 notice: (1) read_dnode: node CRC failed on dnode at 0x1b8000c: read 0xb08d1054, calculated 0x8b624504
JFFS2 warning: (999) jffs2_do_read_inode_internal: no data nodes found for ino #2
Returned error for crccheck of ino #2. Expect badness...
JFFS2 notice: (999) jffs2_get_inode_nodes: Node header CRC failed at 0x1be01ec. {5e78,975c,e5148c7f,d9dfc719}
Node totlen on flash (0xb91b6f6d) != totlen from node ref (0x0000004c)
JFFS2 warning: (999) jffs2_do_read_inode_internal: no data nodes found for ino #4
Returned error for crccheck of ino #4. Expect badness...
JFFS2 notice: (999) jffs2_get_inode_nodes: Node header CRC failed at 0x1be02b4. {5e78,5794,c8e353ef,cbaf9d11}
Node totlen on flash (0x55546c69) != totlen from node ref (0x0000004c)
JFFS2 warning: (999) jffs2_do_read_inode_internal: no data nodes found for ino #5
Returned error for crccheck of ino #5. Expect badness...
JFFS2 notice: (1) read_dnode: node CRC failed on dnode at 0x17be924: read 0x3e803e8, calculated 0x9920efca
JFFS2 notice: (999) jffs2_get_inode_nodes: Node header CRC failed at 0x1be0448. {5e78,d62c,dd943879,5b7007ff}
Node totlen on flash (0xebd63f87) != totlen from node ref (0x0000004c)
JFFS2 warning: (999) jffs2_do_read_inode_internal: no data nodes found for ino #7
Returned error for crccheck of ino #7. Expect badness...
Data CRC d8358eb0 != calculated CRC 0e70dd3e for node at 017591a8
JFFS2 notice: (999) jffs2_get_inode_nodes: Node header CRC failed at 0x1be0510. {5e78,975c,d5956c0f,fbcfc015}
Node totlen on flash (0x5754684f) != totlen from node ref (0x0000004c)
JFFS2 warning: (999) jffs2_do_read_inode_internal: no data nodes found for ino #8
Returned error for crccheck of ino #8. Expect badness...
JFFS2 notice: (999) jffs2_get_inode_nodes: Node header CRC failed at 0x1be05d4. {5e78,d3ac,415b4c21,a3f1c71c}
Node totlen on flash (0x695c686d) != totlen from node ref (0x0000004c)
JFFS2 warning: (999) jffs2_do_read_inode_internal: no data nodes found for ino #9
But I can log into the system. However, when try to execute command like ls, cd, I still see the same error.
JFFS2 notice: (1088) read_dnode: node CRC failed on dnode at 0x1b30474: read 0x3afc5558, calculated 0xb169a063
JFFS2 warning: (1088) jffs2_do_read_inode_internal: no data nodes found for ino #154
iget() failed for ino #154
(none) login: root
login[1088]: root login on 'ttyAM0'
JFFS2 notice: (1088) read_dnode: node CRC failed on dnode at 0x1b4f42c: read 0x000000, calculated 0x28966911
Node totlen on flash (0x00000044) != totlen from node ref (0x000001b4)
~ #
~ # ls
JFFS2 notice: (1088) read_dnode: node CRC failed on dnode at 0x1b50bc8: read 0x1b62df47, calculated 0x3809b5af
JFFS2 notice: (1022) jffs2_get_inode_nodes: Node header CRC failed at 0x16ecd18. {008d,0000,00000000,00000007}
JFFS2 warning: (1088) jffs2_do_read_inode_internal: no data nodes found for ino #90
iget() failed for ino #90
-sh: ls: Input/output error
~ # JFFS2 warning: (1022) jffs2_do_read_inode_internal: no data nodes found for ino #374
Returned error for crccheck of ino #374. Expect badness...
Process of updating firmware is normal, and the kernel partition, ucl.xml is as following
Creating 2 MTD partitions on "mx28_nor_flash":
0x000000000000-0x000000400000 : "kernel" ----total 4M
0x000000400000-0x000002000000 : "rootfs" ----total 28M
<LIST name="SPI-NOR (kernel and rootfs)" desc="zyx test">
<CMD type="boot" body="Recovery" file="updater.sb" if="HabDisable">Booting update firmware.</CMD>
<CMD type="boot" body="Recovery" file="updater_ivt.sb" if="HabEnable">Booting update firmware.</CMD>
<CMD type="find" body="Updater" timeout="180"/>
<CMD type="push" body="mknod class/mtd,mtd0,/dev/mtd0"/>
<CMD type="push" body="mknod class/mtd,mtd1,/dev/mtd1"/>
<CMD type="push" body="mknod block,mtdblock1,/dev/mtdblock1,block"/>
<CMD type="push" body="$ flash_eraseall /dev/mtd0">Erasing kernel partition</CMD>
<CMD type="push" body="send" file="files/imx28_ivt_linux.sb">Sending kernel</CMD>
<CMD type="push" body="$ dd if=$FILE of=/dev/mtd0">Programming kernel</CMD>
<CMD type="push" body="$ flash_eraseall -j /dev/mtd1">Erasing rootfs partition</CMD>
<CMD type="push" body="$ mkdir -p /mnt/mtdblock1"/>
<CMD type="push" body="$ mount -t jffs2 /dev/mtdblock1 /mnt/mtdblock1"/>
<CMD type="push" body="pipe tar -jxv -C /mnt/mtdblock1" file="files/rootfs.tar.bz2">Sending and writting rootfs</CMD>
<CMD type="push" body="frf">Finishing rootfs write</CMD>
<CMD type="push" body="$ umount /mnt/mtdblock1">Unmounting rootfs partition</CMD>
<CMD type="push" body="$ echo Update Complete!">Done</CMD>
</LIST>
Thanks in advance!