i.mx28 No DMA PCM interrupts for SAIF1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx28 No DMA PCM interrupts for SAIF1

1,903 Views
matthevern
Contributor I

We are having an occasional and difficult to reproduce issue on i.mx28 and audio.

We have a custom board and identical connections to SGTL5000. We have SAIF0 setup as

playback and SAIF1 as capture.

What seems to happen is after some random (and usually large) number of attemtps to use 'arecord' for example,

the arecord will freeze and there will only be a 44 byte header file written to a file.

The only way we have found to use the capture again is to reboot.

Dumping /proc/interrupts at this time we can see that there are no 'MXS PCM DMA' interrupts

being generated.

Dumping the SAIF registers at this time shows that.

0x80046000: 0x00000806 (SAIF_CTRL)

0x80046010: 0x80010060 (SAIF_STAT)

0x80046020: 0x00000000 (SAIF_DATA)

0x80046030: 0x01010000 (SAIF_VERSION)

The SAIF_CTRL register shows that the RUN bit clear, and SAIF_STAT shows that

FIFI_OVERFLOW_IRQ, FIFO_UNDERFLOW_IRQ, DMA_PREQ are all set.

We are running based off freescales 2.6.35 git tree

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_maintain

Although we have excluded the 3 SAIF patches previous to the most recent commit, because

we (thought) we found at some point they were causing noise issues for us.

90ce77d ENGR00285446-3 [MX28] SAIF: Bit Shift in SAIF RX Data

1ea685a ENGR00285446-2 [MX28] SAIF: Bit Shift in SAIF RX Data

1ca8992 ENGR00285446-1 [MX28] SAIF: Bit Shift in SAIF RX Data

We also have 1 extra patch from Peter Chan, see

https://community.freescale.com/thread/307611#331003

Although it seems that the the sound/soc/mxs/mxs-pcm.c related changes in this

patch weren't applied. This includes a 'mxs_dma_reset' for the dma channel on

mxs_pcm_close.

Note that in the freescale 2.6.35 git tree mentioned above, this 'mxs_dma_reset' call

isn't present either, and I'm not sure if it should be ?

There seem have some similar issues reported in the past

https://community.freescale.com/message/311756

There is a patch provided on the forum from Peter Chan which addresses an issue which could be similar to what we are seeing

https://community.freescale.com/thread/300291

I can see this patch in the git tree

08f0ca6 ENGR40464722-2 MX28 ALSA: enable the SAIF by toggle the RUN bit

This comment in the patch sounds very similar to what we are seeing:

"The origin method to trigger the SAIF may leads to the DMA hang after runs for 10000 loops of "gplay x.mp4".

However later on this patch is backed out

135155e ENGR00241779: Revert "ENGR40464722 ALSA: enable the SAIF by toggle the RUN bit"

With the comment that "The toggle method could not be applied to mx28evk board, because it use

saif->mclk as mclk of external codec:sgtl5000, saif->mclk is available only when run bit setting"

Does this mean that the basic issue still exists ?

Note that an aplay using the playback device (SAIF0) still works fine when the SAIF1 port

has entered this state.

As far as I can see things seem to be pointing towards some sort of problem related to DMA, does anyone

have any further ideas or suggestions on this ?

Labels (1)
Tags (3)
0 Kudos
Reply
5 Replies

1,148 Views
ftonello
Contributor I

Hi,

I have a similar problem on kernel 4.4 vanilla. A pcm device hangs after some operations to the DMA by plugin and unplugin the USB to a host, for example.

Any information on it?

0 Kudos
Reply

1,148 Views
tomi
Contributor I

hi

anyone found a solution for playback DMA hang problem we have this also we are using kernel 2.6.35

thanks

0 Kudos
Reply

1,148 Views
gusarambula
NXP TechSupport
NXP TechSupport

Please revert the patch at https://community.freescale.com/thread/307611#331003 and https://community.freescale.com/thread/300291

and then re-apply


90ce77d ENGR00285446-3 [MX28] SAIF: Bit Shift in SAIF RX Data

1ea685a ENGR00285446-2 [MX28] SAIF: Bit Shift in SAIF RX Data

1ca8992 ENGR00285446-1 [MX28] SAIF: Bit Shift in SAIF RX Data

The ENGR00285446 patches are the proper solution to resolve the SAIF1 recording issue,

If the noise issues still persists, could you please describe the reproducing steps so that we can follow?

1,148 Views
huangjing
Contributor I

ENGR00285446 DO fix recording issue,but still NOT fix playback "DMA hang" issue.

very big trouble for me now,base on mx28evk hardware,

saif->mclk as mclk of external codec,cant use toggle method...

i have to restart system when sound playback failed,that is too bad.

need help about this issue.

0 Kudos
Reply

1,148 Views
matthevern
Contributor I

Thanks for this clarification.

Unfortunately I don't have access to the particular hardware any more so I will be unable to attempt to reproduce the issue.

0 Kudos
Reply