i.mx27: purpose of osc32k_bypass pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx27: purpose of osc32k_bypass pin

1,120 次查看
bstraehl
Contributor I

Hello

We are working with a quite old hardware here based on the i.mx27 and now I'm wondering what's the purpose of the input pin osc32k_bypass. Could anybody explain?

Thanks in advance.

Best regards,

Beat

标签 (1)
0 项奖励
回复
2 回复数

1,004 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Beat,

When the OSC32K_bypass pin is set to high it instructs that the 32Khz clock will be feed into the processor trough the an external 32khz oscillator connected to the EXTAL32K pin. This is meant for test purposes only so in your application is strongly recommended that the OSC32K_bypass signal is set to 0.

I hope this helps!

Regards,

1,004 次查看
bstraehl
Contributor I

Hello Gusarambula

Yes it helps. Thank you for the clarification.

Regards,

Beat

0 项奖励
回复