i.mx23 connection via ubuntu desktop minicom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx23 connection via ubuntu desktop minicom

2,411 Views
YavuzKaran
Contributor I

Hi,

I'm new to using i.mx23.I have board and its include mini usb.I know mfg tool use this usb port.

First, im using ubuntu 20.04 and connect via usb to i.mx23 board .when check the usb port (lsusb) i can see sigmatel driver.but i can't use minicom.

i want connect imx23 embedded linux and developer software inside.

Maybe i want use rs232 port? but im23 card dont have rs232.

I'm using ubuntu 20.04 and Embedded qt.

Best Regards.

0 Kudos
Reply
2 Replies

2,402 Views
igorpadykov
NXP Employee
NXP Employee

Hi YavuzKaran

 

what board used in the case, if it is based on i.MX233 EVK one can look at

i.MX23 EVK Linux Documentation Bundle

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

Some third parties also develop i.MX233 based boards:

https://www.olimex.com/Products/OLinuXino/iMX233/iMX233-OLinuXino-MICRO/open-source-hardware

 

Best regards
igor

0 Kudos
Reply

2,398 Views
YavuzKaran
Contributor I

Dear Igor ,

Thanks a lot for your quick reply.My product is not evolution board.im using special pcb board and have i.mx23 mcu.I know, my board same character  of i.MX233 EVK board.when load new program for this board, we it like in the link  https://community.nxp.com/t5/i-MX-Processors/How-to-load-image-onto-NAND-flash-at-i-MX23-Evaluation-... .

But i dont have any idea to how to connect via miniusb this board or i.MX233 EVK board.

I will  read the documents you sent.i hope i can find how to connect.

i sent  mfg tool image (loading new program) via attachment

i sent board image 

I will write result.

Thanks a lot for everything.

Regards

0 Kudos
Reply