i.mx 93 TPM timer configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx 93 TPM timer configuration

跳至解决方案
2,117 次查看
Karr
Contributor I

I'm working with a SoM based on the i.mx 9352. I'm looking for a way on how to create a chain of TPM timers in the firmware for the Cortex-M core. In my case, I use TPM6_EXTCLK pin for receiving external clock source from a crystal and then it is used for generating signals on TMP6_CH1, TMP6_CH2 and TMP6_CH3. I want to use TMP6_CH0 as an external source for the TMP5. Is it possible to use an output of the TMP6_CH0 as a an external clock source for TMP5_EXTCLK? Or is this only possible by physically connecting the TMP6_CH0 and TMP5_EXTCLK pins?

Maybe it is possible by using an external trigger source? It is mentioned in the RM for i.mx 93 that I should see the chip-specific TPM information for available external trigger options, but I don't know where to find this information - is it an extra document about i.mx 9352?

标记 (1)
0 项奖励
回复
1 解答
2,072 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Karr 

Thank you for the clarification, I double checked and according the reference manual, there is not a way to do a "trigger" from TPMn to other TPM, it appears it must be a physical connection as you described.

 

Best regards,

--... ...--

Salas.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,104 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Karr 

Look the below Block diagram:

Alejandro_Salas_0-1720738834875.png

 

In chapter 67.3.10.1 Counter Clock mode of reference manual is mentioned:

SC[CMOD] either disables the TPM counter or enables one of the three possible clock sources for the TPM counter. After any reset, SC[CMOD] becomes 0, which disables the TPM counter. You can configure SC[CMOD] for one of the following counter clock sources:


• Asynchronous counter clock
• External clock input pin
• External trigger source


You can read or write to SC[CMOD] at any time. Disabling the TPM counter by writing 0 to SC[CMOD] does not affect the TPM counter value or other registers, but the TPM counter clock domain must acknowledge this disabling action before SC[CMOD] becomes 0.
The external clock input and external trigger source pass through a synchronizer. The TPM counter clock clocks this synchronizer to ensure that counter transitions are properly aligned to counter clock transitions. Therefore, to meet Nyquist criteria, and also considering jitter, the frequency of the external clock source must be less than half of the counter clock frequency.

Also, look the TRGSEL and TRGSRC bits on CONF register (67.7.1.16 Configuration (CONF)).

 

I hope this information can helps to achieve your application.

 

Best regards,

--... ...--

Salas.

 

0 项奖励
回复
2,083 次查看
Karr
Contributor I

Hello @Manuel_Salas,

Thank you for the diagram! I used it to understand how I can clock my TIM6 by an external source, and it is a kind of working now.

My current issue is that I don't know is it possible to clock TIM5 with an output channel of TIM6 (e.g. TIM6_CH0). To illustrate better what I'm trying to build I've made this picture based on your diagram:

TIM6_to_TIM5.jpg

I see that TPM clock can be sourced either by an external clock source (case for TIM6) or by an external trigger source. And I thought that the external trigger source for TIM5 can be an output of the TIM6_CH0. But for now I see only one way how to do that - physically connect TIM6_CH0 pin to the TIM5_EXTCLK pin. Is there are some internal connections inside the MCU, which I can use instead of the physical connection?

So basically I want to have TIM5 and TIM6 been synchronized, and use extra TIM5's channels for sending events based on the TIM6_CH0 output.

0 项奖励
回复
2,073 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Karr 

Thank you for the clarification, I double checked and according the reference manual, there is not a way to do a "trigger" from TPMn to other TPM, it appears it must be a physical connection as you described.

 

Best regards,

--... ...--

Salas.

0 项奖励
回复
2,064 次查看
Karr
Contributor I

Dear @Manuel_Salas ,

Clearly, thank you, then we will think about the physical routing in this case.

But maybe you know where to find the information about the external trigger options for TPM? RM manual for i.mx 93 refers to the chip-specific TPM information, but I cannot find it anywhere:

external_triggers.jpg

 

I've tried to search around the document, but seems this information is not available in the RM.

0 项奖励
回复