i.mx 8M Mini: How to power NVCC_SD2 when not using SD2 interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx 8M Mini: How to power NVCC_SD2 when not using SD2 interface?

ソリューションへジャンプ
1,431件の閲覧回数
adevries
Contributor V

Hello,

I'm using an i.mx 8M Mini in an application where the SD card interface isn't needed. When I was using this interface previously I had the power pin NVCC_SD2 connected up to a voltage rail that could switch between 1.8V and 3.3V.

According to the Hardware Design Guide, NVCC_SD2 should remain powered even if the interface isn't being used. But since the interface isn't being used and doesn't need to switch between 1.8V and 3.3V, is it acceptable to just power NVCC_SD2 with a standard 1.8V or 3.3V rail? Timing-wise, the rail should just power on and off with all the other NVCC_1V8 and NVCC_3V3 GPIO rails, right?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,419件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes one can power NVCC_SD2 with just 1.8V. 1.8V or 3.3V does not matter.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,424件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alexander

 

> Timing-wise, the rail should just power on and off with all the other NVCC_1V8 and NVCC_3V3 GPIO rails, right?

 

yes this is correct.

 

Best regards
igor

0 件の賞賛
返信
1,421件の閲覧回数
adevries
Contributor V

Hi Igor,

Can I power NVCC_SD2 with just 1.8V? Does it matter if I choose 1.8V or 3.3V?

Thanks

0 件の賞賛
返信
1,420件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes one can power NVCC_SD2 with just 1.8V. 1.8V or 3.3V does not matter.

 

Best regards
igor

0 件の賞賛
返信