i.mx 28 evk - where do I get an expansion board to access the I/O?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx 28 evk - where do I get an expansion board to access the I/O?

789 次查看
johnkeates
Contributor I

Am I going mad??

I have the i.mx 28 and i.mx 51 development boards, neither allow access to the I/O except through the expansion board... I can see the expansion port connector but no reference to a connector part number or an expansion board??

标记 (4)
0 项奖励
回复
2 回复数

702 次查看
Yuri
NXP Employee
NXP Employee

  Please accept our apologies, that the documentation it is not quite well explaining

the expansion board ; this option was made for the i.MX28EVK and for the i.MX51EVK. 

You can see an image under the following link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX51EVKJ

If you click in buy/specifications you can find and order the expansion board, which may

be connected to the J53 of the i.MX28EVK board.


Best regards

Yuri

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

702 次查看
igorpadykov
NXP Employee
NXP Employee

Hi John

please check schematic on links below ( under section

"Printed Circuit Boards and Schematics-Schematics"  )

i.MX28 Evaluation Kit|Freescale

i.MX53 Quick Start Board|Freescale

Regarding expansion board, please look at link below

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX51EVKJ

If you click in buy/specifications you can find and order the expansion board, which may

be connected to the J53 of the i.MX28EVK board.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复