i'm facing problem with using yocto for fslimage bitbake.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i'm facing problem with using yocto for fslimage bitbake.

907 次查看
dsfaf
Contributor I

when i use yocto for making linux image, the system shows:

| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_xor_4'

| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_sub_4'

| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_add_4'

| ./.libs/libglib-2.0.so: undefined reference to `__sync_bool_compare_and_swap_4'

| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_or_4'

| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_and_4'

| collect2: ld returned 1 exit status

| make[4]: *** [gtester] Error 1

| make[4]: Leaving directory `/home/zhd/fsl-arm-yocto-bsp/build/tmp/work/i686-linux/glib-2.0-native/1_2.36.4-r0/build/glib'

| make[3]: *** [all-recursive] Error 1

i 've searched the solution on the internet. they said it was caused because of my gcc version.

but i find :

[root@localhost tmp]# yum install gcc

Loaded plugins: fastestmirror

Repository base is listed more than once in the configuration

Repository update is listed more than once in the configuration

Repository addons is listed more than once in the configuration

Repository extras is listed more than once in the configuration

Repository centosplus is listed more than once in the configuration

Repository contrib is listed more than once in the configuration

Repository testing is listed more than once in the configuration

Loading mirror speeds from cached hostfile

* epel: mirror01.idc.hinet.net

Setting up Install Process

Package gcc-4.1.2-55.el5.i386 already installed and latest version

Nothing to do

[root@localhost tmp]#

so i think it's not because of my gcc version.

who can help me?

thanks a lot!

zhong

标签 (3)
0 项奖励
回复
1 回复

785 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Zhong,

Would you please provide more details on your setup? Are you using the FSL BSP Release or the FSl Community BSP and for which board are you building?

0 项奖励
回复
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----