i build the core image minimal by following this link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i build the core image minimal by following this link

632 Views
zubayrbhutta
Contributor I

GitHub - Freescale/fsl-community-bsp-platform: BSP platform manifest. Now i needed a tool chain to compile the programs for imx7dsabresd machine but the error generated after executing the bitbake command is

    class FuncFailed(Exceptionls):
NameError: name 'Exceptionls' is not defined.

Any ideas?

0 Kudos
Reply
1 Reply

565 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Zubayr Bhutta,

Which command are you using to build the toolchain?

$ bitbake meta-toolchain

This should suffice to generate the toolchain installer for your machine.

Would you please include the log file in order to see what recipe is generating an error?

Regards,

0 Kudos
Reply