i build core- ubuntu 16.04(xenial) on imx6 (kernel 3.14.28) ,but booting occur error :[ OK ] Started getty on tty2-tty6 if dbus and logind are not available. [ TIME ] Timed out waiting for device dev-ttymxc0.device. [DEPEND] Dependency failed for Seria

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i build core- ubuntu 16.04(xenial) on imx6 (kernel 3.14.28) ,but booting occur error :[ OK ] Started getty on tty2-tty6 if dbus and logind are not available. [ TIME ] Timed out waiting for device dev-ttymxc0.device. [DEPEND] Dependency failed for Seria

1,136 次查看
tomsen
Contributor I

 [  OK  ] Reached target Login Prompts.

[  OK  ] Reached target Multi-User System.

[  OK  ] Reached target Graphical Interface.          Starting Update UTMP about System Runlevel Changes...

[  OK  ] Started Update UTMP about System Runlevel Changes

then stop.

i already set CONFIG_FHANDLE=y.

what reason?

please help mei! thanks

0 项奖励
回复
1 回复

822 次查看
igorpadykov
NXP Employee
NXP Employee

Hi hw

please refer to

Ubuntu Xenial for i.MX6/7 boards – August 2016 (kernel 4.1.15) - Boundary Devices 

Ubuntu Trusty for i.MX6 boards - December 2015 (kernel 3.14.28) - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复