i.Mx8QXPlus update the boot location of M4 image from A35 Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx8QXPlus update the boot location of M4 image from A35 Linux

418 Views
jithesh77
Contributor I

Hi

Planning to implement firmware upgrade for M4 Core . Is there any method to keep two M4 images in eMMC (one is factory image) and change boot location to factory image from A35 Linux when the current image fails.i.Mx8QXPlus M4 image is starting before uboot.

Thanks

Jithesh

0 Kudos
2 Replies

410 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jithesh

 

unfortunately I am not aware of such special procedures, in general one can look at

sect.5.8.2.2.1 High Level eMMC Boot Flow  i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

0 Kudos

404 Views
jithesh77
Contributor I

Hi Igor,

Thanks for the document. I will confirm.

 

Thanks

Jithesh

0 Kudos