i.Mx8QXPlus M4 Ethernet Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx8QXPlus M4 Ethernet Speed

Jump to solution
1,145 Views
jithesh77
Contributor I

Hi 

If an i.Mx8QXPlus M4 Ethernet is configured for an application use  ,how much will be the maximum speed it supports ,is it 10/100Mbps ? Is it possible to configure it for 1 Gbps . Could you please confirm. 

Thanks

Jithesh

0 Kudos
1 Solution
1,112 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jithesh 

 

yes this is correct understanding.

 

Best regards
igor

View solution in original post

0 Kudos
6 Replies
1,137 Views
jithesh77
Contributor I

Hi Igor

Thanks for the quick response .

M4 Processor runs in 200Mhz is this enough to process the Gigabit ethernet speed. 

Thanks

Jithesh

0 Kudos
1,133 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jithesh

 

these are different modules, running separately one from each other.

Also ENET module has own DMA engine.

 

Best regards
igor

0 Kudos
1,123 Views
jithesh77
Contributor I

Hi Igor,

Thanks for the response.

Here my requirement is to connect 1ENET module to M4  and 1ENET module to A35 Core ,in both case required to get performance of 1 Gigabit maximum. So I can enable DMA parallelly(is it possible ?) in both Cases to get maximum performance. Could you please confirm  my understanding is correct.

Thanks

Jithesh 

0 Kudos
1,113 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jithesh 

 

yes this is correct understanding.

 

Best regards
igor

0 Kudos
1,093 Views
jithesh77
Contributor I

Hi Igor

Thanks for the confirmation.

Thanks

Jithesh

0 Kudos
1,142 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jithesh

 

ENET module perfomance (Ethernet speed) does not depend which core is using it, so max. speed

can be as described in datasheet 1000-Mbit/s.

 

Best regards
igor

0 Kudos