Hi supporter,
My iMx6Q board is runing linux+QT, HDMI and LCD device are connected.
I want to support dual display, and set environment in uboot as follow:
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=lcd,TIANMA050-WVGA@60,bpp=32,if=RGB24 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off ldo_active=on'
LCD can display, but HDMI can't output.
If I change the environment:
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=lcd,TIANMA050-WVGA@60,bpp=32,if=RGB24 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off ldo_active=on'
HDMI can output, but LCD can't display.
Dose it mean that kernel don't support dual display or dual dispaly is implmented by applicantion?
BRs,
Hi nick
please try procedures described in sect.4.7 Running Linux OS on the target
attached Linux Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
I found that LCD and HDMI can display the same content as long as HDMI resolution width is less than 1024.
I have also found the corresponding code in kernel/driver/mxc/ipu3/ipu_disp.c as follow:
void _ipu_dmfc_set_wait4eot(struct ipu_soc *ipu, int dma_chan, int width)
{
...
if (width >= HIGH_RESOLUTION_WIDTH) {
if (dma_chan == 23)
_ipu_dmfc_init(ipu, DMFC_HIGH_RESOLUTION_DP, 0);
else if (dma_chan == 28)
_ipu_dmfc_init(ipu, DMFC_HIGH_RESOLUTION_DC, 0);
}
...
}
HIGH_RESOLUTION_WIDTH equal to 1024 here,
Why do external handler for the width?
BRs,
Nick