i.Mx6 SoloLite BootStrap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx6 SoloLite BootStrap

24,977 Views
pankajrana
Contributor III

Hi,

Referring to the MCIMX6SLEVK schematics, can we remove the ICs U21,U22,U23 and U31 circuitry if not using LCD signals for any other purpose other than Booting ?

I believe we can directly connect the BT_CFG nets to the 4.7KOhm resistors, will it cause any harm ? please comment.

Thanks

--Pankaj Rana

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

24,678 Views
Yuri
NXP Employee
NXP Employee

   From Table 1-2 (EIM recommendations for developer’s boot modes)
of the Hardware Development Guide for i.MX 6SoloLite :

“Isolation buffers are required because 6SoloLite pads

can be set to 1.8V or 3V logic levels while boot signals

require 3V logic level to latch the boot settings.

Any pull-ups for boot configuration line must be properly

isolated because there is a chance that the system may

use 1.8V logic levels.”

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

24,678 Views
pankajrana
Contributor III

Hi Yuri,

I understand that isolation buffers are necessary when the Boot signals are muxed to be used for some other interface as well (say interfacing a LCD to the processor).

"If not using the boot signals (LCD_DAT0 - LCD_DAT23) for any other interface, in that case can we avoid the isolation buffers?"

--Pankaj Rana

0 Kudos
Reply

24,678 Views
Yuri
NXP Employee
NXP Employee

Yes.

0 Kudos
Reply