i.Mx51 2nd display issue in Ubuntu (Kernel 2.6.35.3)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx51 2nd display issue in Ubuntu (Kernel 2.6.35.3)

641 Views
DualDisplayiss1
Contributor I

Hi~~All:

 

 

have anyone porting i.mx51 with Ubuntu 10.04?

 

we're porting Ubuntu 10.04 and kernel version is 2.6.35.3.when boot in 2nd display 800x600 16 bit(RGB565).The Ubuntu display was not good.Bt same parameter are work on wince 6.0 and 7.0.

 

 

{
  /* 800x600 @ 60 Hz , pixel clk @ 40MHz  eric */
  "INNOLUX-SVGA", 60, 800, 600, 25000, 210, 40, 12, 23, 1, 1,
  FB_SYNC_CLK_LAT_FALL,
  FB_VMODE_NONINTERLACED,
  0,},

 

 

Eric

Tags (1)
0 Kudos
2 Replies

565 Views
DualDisplayiss1
Contributor I

OK~~~

 

 

i had done with this issue.

Eric

Campro eric@campro-cctv.com said:

eric@campro-cctv.com

 

if anyone can reply me.plz

0 Kudos

565 Views
DualDisplayiss1
Contributor I

eric@campro-cctv.com

 

if anyone can reply me.plz

0 Kudos