i.Mx28, is there a way to change a device driver without rebuild zImage?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.Mx28, is there a way to change a device driver without rebuild zImage?

1,227件の閲覧回数
jlu
Contributor II

the CAN device driver at 2.6.35 does not output frames in the right order. we have fixed the issue in a later version. now I want to know how to push that fix to older devices already out in the field. 

ラベル(2)
0 件の賞賛
5 返答(返信)

1,101件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jill jlu

I am afraid there is no way to push that fix without rebuilding image.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,101件の閲覧回数
jlu
Contributor II

Hello igor,

Then is there a way to dynamically override a driver? Hard to believe an error in device drivers has to trigger a recall.

Thank you very much,

Jill

0 件の賞賛

1,101件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jill

 

could you clarify for "dynamically override a driver", probably point to some example.

 

Best regards
igor

0 件の賞賛

1,101件の閲覧回数
jlu
Contributor II

Hello igor,

I mean override a driver after zImage has loaded, in anyway. I don't know how to do it. 

Specifically, I use socketcan. In the kernel the socketcan uses can driver; the can driver uses flexcan driver. The flexcan driver has bugs. I am looking for a way to load a new can driver (or flexcan driver) as loadable module and bind the socketcan to this new can driver. This new module will not be in the zImage. How to achieve that?

thank you,

Jill

0 件の賞賛

1,101件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jill

 

I am afraid this is not feasible, sorry.

 

Best regards
igor

0 件の賞賛