i.MX93 m33 GPIO input as interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX93 m33 GPIO input as interrupt

ソリューションへジャンプ
1,130件の閲覧回数
pzab
Contributor II

I would like to use one of the GPIO2 pins as interrupt trigger in CM33 firmware (FreeRTOS) running simultaneously with Linux. Is it possible to use GPIO2 in Linux and in CM33 at the same time?

Is interrupt from GPIO controller supported?

0 件の賞賛
返信
1 解決策
1,094件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @pzab

Thank you for contacting NXP Support.

Could you please help to clarify your question?

As far as I understand you are looking to use GPIO2 as part of the Cortex A and Cortex M at the same time. If it's the case this is not possible, but you can manage the interrupt on Cortex M and send a message to Cortex A.

Have a great day!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,089件の閲覧回数
pzab
Contributor II

This actually answers my question. I was wondering if it is possible to exclude one pin that would be handled by CM33 while the rest would be handled by Linux (A55).

0 件の賞賛
返信
1,095件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @pzab

Thank you for contacting NXP Support.

Could you please help to clarify your question?

As far as I understand you are looking to use GPIO2 as part of the Cortex A and Cortex M at the same time. If it's the case this is not possible, but you can manage the interrupt on Cortex M and send a message to Cortex A.

Have a great day!

0 件の賞賛
返信