Hello,
I observe some flickering and others glitches when trying to setup a parallel LCD with imx93.
I attached a picture of the output of the fb-test command. In the yellow rectangles there are glitches around pixels set to print text "GREEN" and "RED". In the yellow circle there is a glitch, as if lines where pixels were set (for the text) were shifted left.
fb-test output
The framebuffer is configured as XRGB8888 (bpp 32), size 800x480. The bus format is configured as rgb888.
The output of the fbset command is :
mode "800x480-0"
# 0.000 MHz, H: 0.000 kHz, V: 0.000 Hz
geometry 800 480 800 480 32
timings 0 0 0 0 0 0 0
accel true
rgba 8/16,8/8,8/0,0/0
endmode
Device tree node for bus format (MEDIA_BUS_FMT_RGB888_1X24) :
¶llel_disp_fmt {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif>;
fsl,interface-pix-fmt = "rgb888";
status = "okay";
ports {
port@1 {
reg = <1>;
display_out: endpoint {
remote-endpoint = <&panel_in>;
};
};
};
};
Panel configuration :
panel {
compatible = "panel-dpi";
power-supply = <®_vdd_3v3>;
backlight = <&backlight>;
panel-timing {
clock-frequency = <33260000>;
hactive = <800>;
vactive = <480>;
hfront-porch = <40>;
hback-porch = <88>;
hsync-len = <128>;
vfront-porch = <35>;
vback-porch = <8>;
vsync-len = <2>;
de-active = <1>;
pixelclk-active = <1>;
};
port {
panel_in: endpoint {
remote-endpoint = <&display_out>;
};
};
};
&lcdif {
status = "okay";
};
As far as I know I configured things the right way, but maybe I missed something. Could you please advise ?
The driver used is lcdifv3, from linux 6.1.55.
已解决! 转到解答。