i.MX93 Silicone rev A0 and kernel 6.1.36_2.1.0 release

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX93 Silicone rev A0 and kernel 6.1.36_2.1.0 release

1,788件の閲覧回数
wooosaiiii
Contributor III

Hi,

I just tried booting 6.1.36_2.1.0 kernel on the i.MX93 A0 silicone revision, and it crashed during booting. Previous kernel 6.1.22 works OK.

So the question is, is i.MX93 A0 rev still able to use the latest 6.1.36 kernel?

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,764件の閲覧回数
wooosaiiii
Contributor III

@takayuki_ishii 

Thanks for your instructions. 

I am already using A0 container, otherwise I would not be able to boot at all on A0 silicone revision

In my case the issue came from CONFIG_IMX_EL_ENCLAVE=m (6.1.22_2.0.0) and CONFIG_IMX_EL_ENCLAVE=y (6.1.36_2.1.0). 

I already fixed that and can report 6.1.36_2.1.0 still boots on the old A0 silicone

0 件の賞賛
返信

1,752件の閲覧回数
takayuki_ishii
Contributor V

Hello @wooosaiiii ,

Thank you for your response.

 

It seems Linux kernel issue.

In my case, it have no message from serial console.

So, I check the boot image and modify it.

 

Best regards,

Ishii.

0 件の賞賛
返信

1,767件の閲覧回数
takayuki_ishii
Contributor V

Hello @wooosaiiii 

I'm just trying it.

I successfully boot it using the following method.

 

1. first you must finished to build and write SD boot image

 

 $ bitbake imxi-image-full
 $ cd tmp/deploy/...
 $ dd if=imx-image-full-imx9xxx.wic of=/dev/sdx

 

 

2. You must re-build flash.bin with a0 firmware.

  See Linux user manual "4.5.13 How to build imx-boot image by using imx-mkimage".

 

2-1. You must copy "mx93a0-ahab-container.img" to imx-boot image work directory.

 

 $ cd <your bitbake dir>
 $ cd tmp/work/imx93_11x11_lpddr4x_evk-poky-linux/imx-boot/1.0-r0/git/
 $ ls
iMX8DXL                                                   Makefile
iMX8M                                                     mkimage_imx8
iMX8QM                                                    patches
iMX8QX                                                    README
iMX8ULP                                                   SCR-imx-mkimage.txt
iMX9                                                      scripts
imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot  src
LICENSE
 $ cp ../../../../armv8a-mx93-poky-linux/firmware-sentinel/0.11-r0/firmware-sentinel-0.11/mx93a0-ahab-container.img ./iMX9/
 $ ls iMX9
bl31.bin                    mx93a1-ahab-container.img
boot-spl-container.img      scripts
flash.bin                   soc.mak
head.hash                   tee.bin
lpddr4_dmem_1d_v202201.bin  u-boot-atf-container.img
lpddr4_dmem_2d_v202201.bin  u-boot.bin
lpddr4_imem_1d_v202201.bin  u-boot-hash.bin
lpddr4_imem_2d_v202201.bin  u-boot-spl.bin
mx93a0-ahab-container.img   u-boot-spl-ddr.bin

 

 

2-2. rebuild flash.bin with a0 firmware.

 

 $ make SOC=iMX9 REV=A0 flash_singleboot

 

 

2-3 write new "flash.bin" to SD-card.

 

 $ sudo umount /dev/sdx1
 $ sudo umount /dev/sdx2
 $ sudo dd if=iMX9/flash.bin of=/dev/sdx bs=1k seek=32 conv=fsync
 $ sync
 $ sync

 

 

3. Remove SD-Card from card reader, insert it to board and Power On.

 

I hope you are successful.

 

Best regards,

Ishii.